Arduino
  • Products
  • More
Arduino
Arduino Forum 6V DC Motor Battery??
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 419 subscribers
  • Views 2805 views
  • Users 0 members are here
Related

6V DC Motor Battery??

mparmpas122321
mparmpas122321 over 12 years ago

Hey guys! I am electrical engineering student and i have a project running. My supervisor told me to control this motor Pololu - 47:1 Metal Gearmotor 25Dx52L mm with 48 CPR Encoder. It needs 6V supply and has a maximum current of 2.2A. What battery should i use with this motor? If i put 4AA batteries, will they be able to give a 2.2A current if needed? I have searched a lot but people say that a battery can theoretically supply whatever current needed but for different time, according to its mAh capacity. Others say that a battery can handle limited current.

Any help?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +2
    All good advice given by all I would like to simply add to the mix based on your desire to protect the motor and keep things simple Rechargables typically also can output significantly more current than…
  • shabaz
    shabaz over 12 years ago +1
    Hi Manos, 4xAA will be fine. As an elec eng student you should just try it - sometimes it's good to experiment. As for the theory, it's related to battery internal resistance. According to the URL, 2.2A…
  • vaghasiamadhuri
    vaghasiamadhuri over 12 years ago +1
    U can use 5 cell NiMh battery pack or buy 5NiMh cell and connect them in series.... So u will have chargeable battery pack of (5x1.2 = 6 V)... and it ll be low cost too...
Parents
  • vaghasiamadhuri
    0 vaghasiamadhuri over 12 years ago

    U can use 5 cell NiMh battery pack or buy 5NiMh cell and connect them in series.... So u will have chargeable battery pack of (5x1.2 = 6 V)... and it ll be low cost too...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vaghasiamadhuri
    0 vaghasiamadhuri over 12 years ago

    U can use 5 cell NiMh battery pack or buy 5NiMh cell and connect them in series.... So u will have chargeable battery pack of (5x1.2 = 6 V)... and it ll be low cost too...