Arduino
  • Products
  • More
Arduino
Arduino Forum I need help with my arduino controlled laser pointer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 625 views
  • Users 0 members are here
Related

I need help with my arduino controlled laser pointer

e14 Contributor
e14 Contributor over 12 years ago

I have cats and they like lasers so I'v bin working on a 2 servo mechanism that moves the laser up down and side to side, this is controlled by and arduino nano but I don't know why the code isn't working.  pics and code below

 

#include <Servo.h>

 

 

Servo xAxis; //left and right movement of laser

Servo yAxis; //up and down controll of laser

 

 

int posX = 0; //stores posision of x axis servo

int posY = 0; //stores posision of y axis servo

 

 

void setup(){

  xAxis.attach(19); //attaches the x axis servo to pin 19

  yAxis.attach(20); //attaches the y axis servo to pin 20

}

 

 

void loop(){

  xAxis.write(posX); //sets servo to posX var

  yAxis.write(posY); //sets servo to posY var

}

 

posted pics on twitter, they were to large to put right on the post

http://t.co/7VEEE71eDy

  • Sign in to reply
  • Cancel
Parents
  • neilk
    0 neilk over 12 years ago

    Hi Kyle

     

    There isn't much code here for the servos to do anything except sit there at position 0 in both axes.

     

    If you include some code to change the values of posX and posY, do the servos move?

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to neilk

    that code was just to try and get them to move and test them, as of now they move to the left and up when i plug the servos in but, it happens even with out the arduino nano plugged in.  here is a video of that https://www.youtube.com/watch?v=1TG-PE7jwXg&feature=youtu.be .   that was a 6 volt supply (4 AA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to neilk

    that code was just to try and get them to move and test them, as of now they move to the left and up when i plug the servos in but, it happens even with out the arduino nano plugged in.  here is a video of that https://www.youtube.com/watch?v=1TG-PE7jwXg&feature=youtu.be .   that was a 6 volt supply (4 AA)