Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum How to use two motors simultaneously with an Arduino uno
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 7 answers
  • Subscribers 423 subscribers
  • Views 4693 views
  • Users 0 members are here
Related

How to use two motors simultaneously with an Arduino uno

e14 Contributor
e14 Contributor over 12 years ago

Hi,

 

I am having trouble making two DC motors work simultaneously working with the Arduino Uno. One motor on its own works fine but both of them do not work together. It would be nice if someone could help me with the circuit and the code.

 

Thanks in Advance,

Ramgopal

  • Sign in to reply
  • Cancel

Top Replies

  • vish
    vish over 12 years ago +2 suggested
    Hi Ram, If I want to control two motors, I will go for a driver circuit. One best solution is to use a motor driver IC. L293D is one of the inexpensive yet excellent ICs for this purpose. You will be able…
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor +1 suggested
    Based on the diagram, you may be overloading the 5v rail of the arduino, it is not designed to supply the load to two motors. Try powering the motors from a desperate supply, only share a common ground…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to nschreiber0813 +1
    Thank you all. I will look at using another battery for powering the motors. Will also look at the L293D. I will get back if I am still facing issues Ram
Parents
  • vish
    0 vish over 12 years ago

    Hi Ram,

    If I want to control two motors, I will go for a driver circuit. One best solution is to use a motor driver IC. L293D is one of the inexpensive yet excellent ICs for this purpose. You will be able to pick up one form your nearest electronics shop for around Rs 60( if u r in India). I have used them in my robotics projects. Also this IC has protection circuits for back emf, so no worries about frying your arduino.

    If you can dedicate two GPIO pins per motor, you will be able to control the motor in both directions. If you can afford only one GPIO, then you can ground the other input pin in L293D and control the motor with just start/stop functionality.

    You can find a good tutorial about interfacing arduino with motors using L293D here ;

    Control a DC motor with Arduino and L293D chip

    Control your motors with L293D and Arduino

     

    -vish

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • vish
    0 vish over 12 years ago

    Hi Ram,

    If I want to control two motors, I will go for a driver circuit. One best solution is to use a motor driver IC. L293D is one of the inexpensive yet excellent ICs for this purpose. You will be able to pick up one form your nearest electronics shop for around Rs 60( if u r in India). I have used them in my robotics projects. Also this IC has protection circuits for back emf, so no worries about frying your arduino.

    If you can dedicate two GPIO pins per motor, you will be able to control the motor in both directions. If you can afford only one GPIO, then you can ground the other input pin in L293D and control the motor with just start/stop functionality.

    You can find a good tutorial about interfacing arduino with motors using L293D here ;

    Control a DC motor with Arduino and L293D chip

    Control your motors with L293D and Arduino

     

    -vish

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer