Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum How to use two motors simultaneously with an Arduino uno
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 7 answers
  • Subscribers 423 subscribers
  • Views 4693 views
  • Users 0 members are here
Related

How to use two motors simultaneously with an Arduino uno

e14 Contributor
e14 Contributor over 12 years ago

Hi,

 

I am having trouble making two DC motors work simultaneously working with the Arduino Uno. One motor on its own works fine but both of them do not work together. It would be nice if someone could help me with the circuit and the code.

 

Thanks in Advance,

Ramgopal

  • Sign in to reply
  • Cancel

Top Replies

  • vish
    vish over 12 years ago +2 suggested
    Hi Ram, If I want to control two motors, I will go for a driver circuit. One best solution is to use a motor driver IC. L293D is one of the inexpensive yet excellent ICs for this purpose. You will be able…
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor +1 suggested
    Based on the diagram, you may be overloading the 5v rail of the arduino, it is not designed to supply the load to two motors. Try powering the motors from a desperate supply, only share a common ground…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to nschreiber0813 +1
    Thank you all. I will look at using another battery for powering the motors. Will also look at the L293D. I will get back if I am still facing issues Ram
  • jomoenginer
    0 jomoenginer over 8 years ago in reply to jbecks

    This is an old thread, however if you are just looking to control 2 DC motors, then you could just add a second definition for the second motor and then just turn both on for forward motion, or turn each off for left and right action.  the best bet is to add a driver transistor for each motor and use it as a switch which will allow you to not over draw the current from the Arduino GPIO pins.

    Something like the follow would work nicely and all you would have to do is duplicate the circuit and GPIO pin definition for the second motor:

    https://www.arduino.cc/en/Tutorial/TransistorMotorControl

     

    However, if you are looking for some forward and backward action with the motor, then you would have to build an H-bridge or by a Motor Shield which will give you more control of the motor movement.

    The Adafruit TB6612 Breakout board is an inexpensive H-Bridge that can control 2 DC Motors.

    https://www.adafruit.com/product/2448?gclid=Cj0KCQjw2KHWBRC2ARIsAJD_r3fSQvAKYUfufOVrEnXzuht1tRHnaku1np6bdeKDh9G_pJFtiXtVgtcaAuNKEALw_wcB

     

    Or you can DIY it with a L293D Quad Half-H Bridge

    http://www.ti.com/product/L293D

     

    This might help answer some questions, or raise new ones:

    https://www.element14.com/community/docs/DOC-89005#comment-127024

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ussengineers
    0 ussengineers over 8 years ago in reply to dragonstyne

    Yep I agree, although arduino's are great they struggle for supply power hungry circuitry such as motors. It is very easy to solve this by using a driver circuit, which can be as simple as a transistor, connect the base to the arduino for control, connect the collector to an external power supply, such as a 9V battery and connect the emitter to ground via a resistor, should supply enough current to keep everything moving!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<