Arduino
  • Products
  • More
Arduino
Arduino Forum I need help with switching signals
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 418 subscribers
  • Views 1314 views
  • Users 0 members are here
  • pins
  • signals
  • switch
Related

I need help with switching signals

e14 Contributor
e14 Contributor over 12 years ago

Hi there

Although I know a thing or two (ok, maybe 1.5 things) about soldering, I am fairly new to this electronics thing. I've been thinking about starting a secret project that I will only share once I finish. I had trouble finding the materials I need such as the battery, the charging mechanism, ...etc. That is not important right now. As I was listing down the things I wanted it to do, I encountered something I don't know how to solve, thus I need your guys' help

Say I'm connecting two points together (let's call them A and B). Now, I need to switch the output from B to another point called D that gets it's signal from point C by pressing a button. Basically I want to flip the signals (you can think of it as cross multiply in math terms) Now you could say "just use a slide switch, you dummy" but the problem is I have 60 inputs and outputs. do you think you can help me with this?

I thought of using an EEPROM because they have a lot of pins so that I would only need to use 2 of them, but I know nothing on how to program them. I would assume a micro controller would be better but I don't know how to program it either, and I assume it's not as cheap as an EEPROM. I also have no experience in using an arduino. I do, however, know the basics of java, so if that helps please tell me

I really wanna do this. I've been thinking about it for quite a while. Please help.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    What you need is a switch or a multiplexer, providing your signals are logic levels, this should work look at something like this : for digital signals use a 74157 (No uProc needed) http://mazharlaliwala…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    like I said in my latest post, the signals are digital. At least I think so.
    the 60 pins actually come from a console. an NES to be exact. I believe the reason why I want to do this is self explanatory for those who know a little about the console

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    I just noticed that they were digital and was editing my reply when you answered.

     

    What sort of signals are they - voltage levels, speed etc. An I know a fair bit about electronics but nothing at all about 'consoles' or even what an 'NES' is - so you need to explain.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelkellett

    honestly, I don't know. As I explained, I am not that good with electronics. I figured that all signals would all be the same since they're (according to my understanding) just a series of binary numbers. I can provide you with the names of the pins, if that helps

     

    Basically, what happens with a cartridge based console, is the console powers up the cartridge with (in the case of the Nintendo Entertainment System aka NES) 5V, and then the cartridge sends signals from two EEPROMs on it to the console.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    You still haven't explained what you want to do !

     

    If it's 5V logic (and it could be because the NES is such old technology) then you can forget about FPGA's because they won't work with 5V.

     

    Are you trying to select between two different cartridges -  if so it may well not be necessary to switch all the signals but just make sure that only one cartridge is enabled at a time.

     

    If you can explain what you are trying to make or do it may be possible to help.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    You still haven't explained what you want to do !

     

    If it's 5V logic (and it could be because the NES is such old technology) then you can forget about FPGA's because they won't work with 5V.

     

    Are you trying to select between two different cartridges -  if so it may well not be necessary to switch all the signals but just make sure that only one cartridge is enabled at a time.

     

    If you can explain what you are trying to make or do it may be possible to help.

     

    MK