Arduino
  • Products
  • More
Arduino
Arduino Forum I need help with switching signals
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 418 subscribers
  • Views 1303 views
  • Users 0 members are here
  • pins
  • signals
  • switch
Related

I need help with switching signals

e14 Contributor
e14 Contributor over 12 years ago

Hi there

Although I know a thing or two (ok, maybe 1.5 things) about soldering, I am fairly new to this electronics thing. I've been thinking about starting a secret project that I will only share once I finish. I had trouble finding the materials I need such as the battery, the charging mechanism, ...etc. That is not important right now. As I was listing down the things I wanted it to do, I encountered something I don't know how to solve, thus I need your guys' help

Say I'm connecting two points together (let's call them A and B). Now, I need to switch the output from B to another point called D that gets it's signal from point C by pressing a button. Basically I want to flip the signals (you can think of it as cross multiply in math terms) Now you could say "just use a slide switch, you dummy" but the problem is I have 60 inputs and outputs. do you think you can help me with this?

I thought of using an EEPROM because they have a lot of pins so that I would only need to use 2 of them, but I know nothing on how to program them. I would assume a micro controller would be better but I don't know how to program it either, and I assume it's not as cheap as an EEPROM. I also have no experience in using an arduino. I do, however, know the basics of java, so if that helps please tell me

I really wanna do this. I've been thinking about it for quite a while. Please help.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    What you need is a switch or a multiplexer, providing your signals are logic levels, this should work look at something like this : for digital signals use a 74157 (No uProc needed) http://mazharlaliwala…
Parents
  • jw0752
    0 jw0752 over 12 years ago

    Hi Ehab,  The diagram was excellent and should get us some help from one of the more experienced guys on the forum. Each element of your switch looks like a cross wired DPDT switch. The only chip I am aware of that has this type of switch is an AD7512 (I've worked with this one) and it only has one DPDT so you would need 30 of them. The AD7512 is a bidirectional analog switch. It has about 75 ohms of internal resistance and can switch about 20 mA. Hopefully there is a chip with internal design to do this specifically on a larger scale. Your clarification should help to get a better answer than I can give you.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to jw0752

    Since the signals are digital it can be done easily with an FPGA.

     

    You will need one with at least 128 useable IO pins, 120 for the switch IO and some for control.

    (Or possibly 2 because then they might be in more manageable packages.)

     

    Can you explain a bit more about what this is for because it may be that there is a much simpler solution if we understood a bit more.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to jw0752

    Since the signals are digital it can be done easily with an FPGA.

     

    You will need one with at least 128 useable IO pins, 120 for the switch IO and some for control.

    (Or possibly 2 because then they might be in more manageable packages.)

     

    Can you explain a bit more about what this is for because it may be that there is a much simpler solution if we understood a bit more.

     

    MK