Arduino
  • Products
  • More
Arduino
Arduino Forum I need help with switching signals
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 418 subscribers
  • Views 1305 views
  • Users 0 members are here
  • pins
  • signals
  • switch
Related

I need help with switching signals

e14 Contributor
e14 Contributor over 12 years ago

Hi there

Although I know a thing or two (ok, maybe 1.5 things) about soldering, I am fairly new to this electronics thing. I've been thinking about starting a secret project that I will only share once I finish. I had trouble finding the materials I need such as the battery, the charging mechanism, ...etc. That is not important right now. As I was listing down the things I wanted it to do, I encountered something I don't know how to solve, thus I need your guys' help

Say I'm connecting two points together (let's call them A and B). Now, I need to switch the output from B to another point called D that gets it's signal from point C by pressing a button. Basically I want to flip the signals (you can think of it as cross multiply in math terms) Now you could say "just use a slide switch, you dummy" but the problem is I have 60 inputs and outputs. do you think you can help me with this?

I thought of using an EEPROM because they have a lot of pins so that I would only need to use 2 of them, but I know nothing on how to program them. I would assume a micro controller would be better but I don't know how to program it either, and I assume it's not as cheap as an EEPROM. I also have no experience in using an arduino. I do, however, know the basics of java, so if that helps please tell me

I really wanna do this. I've been thinking about it for quite a while. Please help.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    What you need is a switch or a multiplexer, providing your signals are logic levels, this should work look at something like this : for digital signals use a 74157 (No uProc needed) http://mazharlaliwala…
Parents
  • jw0752
    0 jw0752 over 12 years ago

    Hi Ehab,  I would suspect that the nes design requires a hard contact between the cartridges and the console. What you want to do would have to be done with 30 DPDT relays. Each relay would flip 2 lines. If you have the pin out names you would have to make sure that "A' goes to "A". I suspect that Michael is right when he says that perhaps not all the lines have to be flipped but could both be hooked up simultaneously.  Without a lot more knowledge of the design the best bet would probably be to just get the hardware and switch them all.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 12 years ago

    Hi Ehab,  I would suspect that the nes design requires a hard contact between the cartridges and the console. What you want to do would have to be done with 30 DPDT relays. Each relay would flip 2 lines. If you have the pin out names you would have to make sure that "A' goes to "A". I suspect that Michael is right when he says that perhaps not all the lines have to be flipped but could both be hooked up simultaneously.  Without a lot more knowledge of the design the best bet would probably be to just get the hardware and switch them all.

    John