Arduino
  • Products
  • More
Arduino
Arduino Forum how to have anologue input and while loop?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 417 subscribers
  • Views 767 views
  • Users 0 members are here
Related

how to have anologue input and while loop?

e14 Contributor
e14 Contributor over 12 years ago

I have a program with a joystick and a LCD. The joystick controls "!"s on the LCD(makes them appear in different places. The joystick if made from potentiometers and when the value gets to a certain point a "!" is suppose to appear on a part of the screen using a while loop. When the value reaches the point to show a "!" on the screen the while loop starts and stops the anologue input from the potentiometers. This makes the value constant forever and the "!" never goes away. An IF statement hasn't worked because i need to clear the screen if the value is not correct for that "!" and that makes it impossible for other "!"s never appear. Are there any solutions to this or other ways of going about it? I am inexperienced so I am in much need of help. (BTW the code is made for four different potentiometers (Two joysticks) but I an only using one joystick (so two potentiometers, sensePinOrange with val1, and, sensePinYellow with val).) CODE:

 

#include <LiquidCrystal.h>

LiquidCrystal lcd(12, 11, 5, 4, 3, 2);

 

 

int sensePinYellow =0;

int sensePinOrange =1;

int sensePinBrown =2;

int sensePinBlue =3;

int val = 0;

int val1 = 0;

int val2 = 0;

int val3 = 0;

 

 

void setup() {

  analogReference(DEFAULT);

  Serial.begin(9600);

 

  lcd.begin(16, 2);

 

 

}

void loop() {

    val = analogRead(sensePinYellow);

    val1 = analogRead(sensePinOrange);

    val2 = analogRead(sensePinBrown);

    val3 = analogRead(sensePinBlue);

    Serial. print(" Yellow=");

    Serial. print(val); /*930=right 210=left */

    Serial. print(" Orange=");

    Serial. print(val1); //925=maxup 195=mindown

    Serial. print(" Brown=");

    Serial. print(val2); //930=right 180=left

    Serial. print(" Blue=");

    Serial. println(val3); //920=maxup 150=mindown

    delay(50);

   

    while (val > 700) {

      lcd.setCursor(15,1); //right

      lcd.print("!");

    }

    while (val < 400) {

      lcd.setCursor(0,1); //left

      lcd.print("!");

    }

    while (val1 > 700) {

      lcd.setCursor(9,0); //up

      lcd.print("!");

    }

    while (val < 400) {

      lcd.setCursor(9,1); //down

      lcd.print("!");

    }

   

}

  • Sign in to reply
  • Cancel
Parents
  • michaelwylie
    0 michaelwylie over 12 years ago

    I would think about it as looking for a change.

    if(cursor changed)

    {

         clear all cursors

         write proper cursors

    }

    The harder part is determining if there was a change. So, think about keeping track of the previous values and comparing them to the newest read ones. If they are different (within tolerance) there was a change. Try thinking about this, and if you can't figure it out, come back an update this post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelwylie
    0 michaelwylie over 12 years ago

    I would think about it as looking for a change.

    if(cursor changed)

    {

         clear all cursors

         write proper cursors

    }

    The harder part is determining if there was a change. So, think about keeping track of the previous values and comparing them to the newest read ones. If they are different (within tolerance) there was a change. Try thinking about this, and if you can't figure it out, come back an update this post.