Arduino
  • Products
  • More
Arduino
Arduino Forum limit switches within a counter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 3084 views
  • Users 0 members are here
Related

limit switches within a counter

e14 Contributor
e14 Contributor over 12 years ago

Hi folks,

Im a technology teacher in Scotland and the powers above have decided that we move from our old PBASIC run Stamp boards, and use Arduino. It has also been decided this will start of next month! this means during my holidays I have been left with no choice but to learn the language and how it works myself, but to create a scheme of work for my pupils to follow. Most of what Ive done is based on Jeremy Blums brilliant online tutorials , and things that are different I was mostly able to work out by looking up.

 

I have came across a problem though and for the life of my I cant seem to solve it and I was hoping someone on here could help! Ive designed a project of dancing ballerina toy (my feeble attempts to try and get more girls into Engineering). When a master switch is pressed, it will put on an ultabrite LED to act as a spotlight for the dancer. The ballerina will then "dance" by sitting on top of a turntable that will rotate one way until it hits a limit switch. When it hits this limit switch it will rotate the other direction until it hits another limit switch, sending it back the original direction. This dancing will repeat 5 times, then everything will switch off.

 

This is a flowchart of what I'm attempting to do, which will hopefully make things a little clearer:

 

image

 

This is how I have wired up my Arduino Uno:

 

image

 

and this is my attempt at the code. It was originally more complicated added in debouncing and commands to keep outputs on once the switches have been presssed, but I deleted all that to try and work out what is going wrong.

 

/*

dancing toy System

*/

 

int MasterSwitchPin = 13;      // Master switch

int LeftSwitchPin = 12;        // Makes motor turn left

int RightSwitchPin = 8;        // Makes motor turn right

int Motor1APin = 7;            // H-bridge leg 1

int Motor2APin = 6;            // H-bridge leg 2

int LEDPin = 2;                // LED

 

 

void setup()

{

  Serial.begin(9600);

  pinMode (MasterSwitchPin, INPUT);

  pinMode (LeftSwitchPin, INPUT);

  pinMode (RightSwitchPin, INPUT);

  pinMode (Motor1APin, OUTPUT);

  pinMode (Motor2APin, OUTPUT);

  pinMode (LEDPin, OUTPUT);

}

 

void loop()

{

   if (digitalRead(MasterSwitchPin) == HIGH)

     {

       digitalWrite(LEDPin, HIGH);

     }

     Serial.print("button pressed LED on");

for (int counter = 1 ; counter <= 5; counter = counter +1) 

   { 

    while (digitalRead(LeftSwitchPin) == HIGH)

      {

      digitalWrite(Motor1APin, HIGH);

      digitalWrite(Motor2APin, LOW);

      Serial.print("motor goes one way");

      }      

      delay(1000);

   

    while (digitalRead(RightSwitchPin) == HIGH)

      {

      digitalWrite(Motor1APin, LOW);

      digitalWrite(Motor2APin, HIGH);

      Serial.print("motor goes the other wat way");

      }

  delay(1000);     

   }

   Serial.print("repeated 5 times");

       digitalWrite(LEDPin, LOW);

       digitalWrite(Motor1APin, LOW);

       digitalWrite(Motor2APin, LOW);

       Serial.print("switch everything off");

}

 

 

can anyone help me please and fix my code? thanks in advance!!!

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 12 years ago

    Hi Paul,

     

    Hopefully someone may respond sooner with better info (busy day for me today unfortunately for the next few hours, so this is a quick reply), but I had a few questions/suggestions:

    1. What is the current symptom? Does any of it function, e.g. does LED turn on, does it stay on, etc. Does button detection work? Does the motor appear to get energised slightly?

    2. Could you try powering the SNxxx chip from a separate supply, not from the Arduino board supply? To see what happens?

    3. Could you place a 100uF capacitor across the supply rails close to the SNxxxx chip, and also a 100nF capacitor across the supply rails close to the chip too?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to shabaz

    Also,

    Just noticed, you've got the digitalWrite commands in the while(digitalread...) statements, but you can move them to just above. The digitalWrite is sustained indefinitely until you do another digitalWrite to the same pin.

    Also, before each delay(1000) line, you need to do a digitalWrite that will switch off the motors, so that for the 1000millisec delay, the motors are not moving.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 12 years ago in reply to shabaz

    Also,

    Just noticed, you've got the digitalWrite commands in the while(digitalread...) statements, but you can move them to just above. The digitalWrite is sustained indefinitely until you do another digitalWrite to the same pin.

    Also, before each delay(1000) line, you need to do a digitalWrite that will switch off the motors, so that for the 1000millisec delay, the motors are not moving.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer