Arduino
  • Products
  • More
Arduino
Arduino Forum limit switches within a counter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 3078 views
  • Users 0 members are here
Related

limit switches within a counter

e14 Contributor
e14 Contributor over 12 years ago

Hi folks,

Im a technology teacher in Scotland and the powers above have decided that we move from our old PBASIC run Stamp boards, and use Arduino. It has also been decided this will start of next month! this means during my holidays I have been left with no choice but to learn the language and how it works myself, but to create a scheme of work for my pupils to follow. Most of what Ive done is based on Jeremy Blums brilliant online tutorials , and things that are different I was mostly able to work out by looking up.

 

I have came across a problem though and for the life of my I cant seem to solve it and I was hoping someone on here could help! Ive designed a project of dancing ballerina toy (my feeble attempts to try and get more girls into Engineering). When a master switch is pressed, it will put on an ultabrite LED to act as a spotlight for the dancer. The ballerina will then "dance" by sitting on top of a turntable that will rotate one way until it hits a limit switch. When it hits this limit switch it will rotate the other direction until it hits another limit switch, sending it back the original direction. This dancing will repeat 5 times, then everything will switch off.

 

This is a flowchart of what I'm attempting to do, which will hopefully make things a little clearer:

 

image

 

This is how I have wired up my Arduino Uno:

 

image

 

and this is my attempt at the code. It was originally more complicated added in debouncing and commands to keep outputs on once the switches have been presssed, but I deleted all that to try and work out what is going wrong.

 

/*

dancing toy System

*/

 

int MasterSwitchPin = 13;      // Master switch

int LeftSwitchPin = 12;        // Makes motor turn left

int RightSwitchPin = 8;        // Makes motor turn right

int Motor1APin = 7;            // H-bridge leg 1

int Motor2APin = 6;            // H-bridge leg 2

int LEDPin = 2;                // LED

 

 

void setup()

{

  Serial.begin(9600);

  pinMode (MasterSwitchPin, INPUT);

  pinMode (LeftSwitchPin, INPUT);

  pinMode (RightSwitchPin, INPUT);

  pinMode (Motor1APin, OUTPUT);

  pinMode (Motor2APin, OUTPUT);

  pinMode (LEDPin, OUTPUT);

}

 

void loop()

{

   if (digitalRead(MasterSwitchPin) == HIGH)

     {

       digitalWrite(LEDPin, HIGH);

     }

     Serial.print("button pressed LED on");

for (int counter = 1 ; counter <= 5; counter = counter +1) 

   { 

    while (digitalRead(LeftSwitchPin) == HIGH)

      {

      digitalWrite(Motor1APin, HIGH);

      digitalWrite(Motor2APin, LOW);

      Serial.print("motor goes one way");

      }      

      delay(1000);

   

    while (digitalRead(RightSwitchPin) == HIGH)

      {

      digitalWrite(Motor1APin, LOW);

      digitalWrite(Motor2APin, HIGH);

      Serial.print("motor goes the other wat way");

      }

  delay(1000);     

   }

   Serial.print("repeated 5 times");

       digitalWrite(LEDPin, LOW);

       digitalWrite(Motor1APin, LOW);

       digitalWrite(Motor2APin, LOW);

       Serial.print("switch everything off");

}

 

 

can anyone help me please and fix my code? thanks in advance!!!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thank you guys for your help - it works! As I said previously I am a beginner at this (but expected to become an expert within a few weeks as I have to teach this stuff to certificate level classes) and you were of great help! This has made it so much easier

     

    .... I did not know about the #define command too so that is of help for the future too. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thank you guys for your help - it works! As I said previously I am a beginner at this (but expected to become an expert within a few weeks as I have to teach this stuff to certificate level classes) and you were of great help! This has made it so much easier

     

    .... I did not know about the #define command too so that is of help for the future too. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    Hi Paul,

     

    Great! Glad it's sorted. Good luck with the rest of your training : )