Arduino
  • Products
  • More
Arduino
Arduino Forum Controlling AC fan
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 2 answers
  • Subscribers 420 subscribers
  • Views 3639 views
  • Users 0 members are here
Related

Controlling AC fan

e14 Contributor
e14 Contributor over 12 years ago

Hello I found these project online its called vent a garage. It has 2 ac fans the LINK DEPOT 120mm AC Cooling Fan (AC-FAN-1238B) and its controlled by a thermostate. What I have plan is to use the arduino  and a temperature sensor to turn on the fans when for example reaches 70 degrees. what I dont know is what to use to link the 2 ac fans to the arduino to communicate.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Ohh man thanks guys for the input. I have only deal with dc and small projects but never mess with ac only when i did my power supply for school project. Peter that Beefcake relay wil boost 5 vt to outputing 220 VAC or it has a seperate connector to plug into ac power

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 12 years ago in reply to e14 Contributor

    Hi Bernardo, The arduino will control the relays on the relay board. The relays are like isolated switches. The 220 volts mentioned does not come from the relay board or the arduino but is just the maximum voltage recommend to be used on the relay switches. You have to supply the power to run the fans from the line voltage power of your house. This voltage can be very dangerous and can be fatal so if you are a beginner get some help from an electrician if you plan to mess with it. The switches in the relays of the relay board can be used to switch on and off any external circuit that they are in series with as long as that circuit has a voltage less than 220V and isn't so big that it consumes more power than the relays can handle.

     

    A wise man I knew once told me that he knew only two things about electricity.

    #1 If you don't pay your bill they turn it off.

    #2 If you mess with it, it kills you.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 12 years ago in reply to e14 Contributor

    Hi Bernardo, The arduino will control the relays on the relay board. The relays are like isolated switches. The 220 volts mentioned does not come from the relay board or the arduino but is just the maximum voltage recommend to be used on the relay switches. You have to supply the power to run the fans from the line voltage power of your house. This voltage can be very dangerous and can be fatal so if you are a beginner get some help from an electrician if you plan to mess with it. The switches in the relays of the relay board can be used to switch on and off any external circuit that they are in series with as long as that circuit has a voltage less than 220V and isn't so big that it consumes more power than the relays can handle.

     

    A wise man I knew once told me that he knew only two things about electricity.

    #1 If you don't pay your bill they turn it off.

    #2 If you mess with it, it kills you.

     

    John