Arduino
  • Products
  • More
Arduino
Arduino Forum Controlling AC fan
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 2 answers
  • Subscribers 420 subscribers
  • Views 3639 views
  • Users 0 members are here
Related

Controlling AC fan

e14 Contributor
e14 Contributor over 12 years ago

Hello I found these project online its called vent a garage. It has 2 ac fans the LINK DEPOT 120mm AC Cooling Fan (AC-FAN-1238B) and its controlled by a thermostate. What I have plan is to use the arduino  and a temperature sensor to turn on the fans when for example reaches 70 degrees. what I dont know is what to use to link the 2 ac fans to the arduino to communicate.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Ohh man thanks guys for the input. I have only deal with dc and small projects but never mess with ac only when i did my power supply for school project. Peter that Beefcake relay wil boost 5 vt to outputing 220 VAC or it has a seperate connector to plug into ac power

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    It has a seep rate connector that is used to control the mains powered devices

     

    one side is for control by the 5v device, the other end acts as a switch for your fans, so live from mains to one connector, the other connector goes to fan and the remaining fan wire back to neutral

     

    the same as if you were simply wiring in a switch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    It has a seep rate connector that is used to control the mains powered devices

     

    one side is for control by the 5v device, the other end acts as a switch for your fans, so live from mains to one connector, the other connector goes to fan and the remaining fan wire back to neutral

     

    the same as if you were simply wiring in a switch