Arduino
  • Products
  • More
Arduino
Arduino Forum Controlling AC fan
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 2 answers
  • Subscribers 420 subscribers
  • Views 3650 views
  • Users 0 members are here
Related

Controlling AC fan

e14 Contributor
e14 Contributor over 12 years ago

Hello I found these project online its called vent a garage. It has 2 ac fans the LINK DEPOT 120mm AC Cooling Fan (AC-FAN-1238B) and its controlled by a thermostate. What I have plan is to use the arduino  and a temperature sensor to turn on the fans when for example reaches 70 degrees. what I dont know is what to use to link the 2 ac fans to the arduino to communicate.

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    these are the spark fun instructions

     

    https://www.sparkfun.com/tutorials/119

     

    But I do agree, If your not familiar and comfortable working with mains voltages, GET HELP, knowledgeable help, professional help if needed. image THIS CAN KILL YOU IF NOT DONE RIGHT  image  

     

    You get to do things right as long as you do them right, in many cases you get to do things wrong only once...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to Robert Peter Oakes

    I hate it when tutorials provide advise that is less than SAFE.

     

    image

     

    The above is WRONG.

    1. It needs to be fastened and NOT floating around.

    2. The wires should not be soldered before entry into a compression style connection, as if there is any heating the solder retract and the connection become poor.

        it either makes it worse or potentially hazardous.

    3. they don't show any form of cable clamp to stop it getting pulled out the box.

    4. The board design leaves a lot to be desired.

        They are relying on a clearance across the pcb of slightly under 2mm ... it should have a physical cut between the track carrying mains voltage and the relay coil.

         (they have put the low voltage side on the other side of the pcb which is wise)

     

    image

     

     

    I agree with the other replies.

    If you are unfamiliar with this then remain unfamiliar and buy something like this which can be controlled remotely from an Arduino.

     

    Easy Off Sockets

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 12 years ago in reply to Robert Peter Oakes

    I hate it when tutorials provide advise that is less than SAFE.

     

    image

     

    The above is WRONG.

    1. It needs to be fastened and NOT floating around.

    2. The wires should not be soldered before entry into a compression style connection, as if there is any heating the solder retract and the connection become poor.

        it either makes it worse or potentially hazardous.

    3. they don't show any form of cable clamp to stop it getting pulled out the box.

    4. The board design leaves a lot to be desired.

        They are relying on a clearance across the pcb of slightly under 2mm ... it should have a physical cut between the track carrying mains voltage and the relay coil.

         (they have put the low voltage side on the other side of the pcb which is wise)

     

    image

     

     

    I agree with the other replies.

    If you are unfamiliar with this then remain unfamiliar and buy something like this which can be controlled remotely from an Arduino.

     

    Easy Off Sockets

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to mcb1

    Agree with most points.

     

    For strain relief, there is built in strain relief on the box, if you look carefully you will see it In the picture

    http://www.sparkfun.com/tutorial/Outlet/Outlet-0.jpg

     

    Top left corner, it is north American box and outlet. NOW the strain relief is not meant for a box left floating un attached. It is for when it is mounted on a stud and with drywall etc around it so in this case it will not be adequate, this is a common misunderstanding over here

     

    should be something more like this

    image

     

    or something from this set of images appropriate to your region https://www.google.ca/search?q=power+cable+strain+relief&espv=2&tbm=isch&tbo=u&source=univ&sa=X&ei=LdPnU-uNLIyYyASGsoHwA…

     

    The socket is good for USA and Canada, not UK or Europe or pretty much any other country (You know what your sockets look like.

     

    Also, if your going to do this, don't do this board, it is not worth it and as MCB pointed out, it has issues

     

    This one from Spark fun is not expensive, seems to be designed much better and has appropriate cable connectors suitable for the job 

     

    Oh and going solid state all the way with something like this https://www.sparkfun.com/products/11042

    https://www.sparkfun.com/products/13015

    image

    This unit requires nothing else, you can control it directly from an Arduino or any other micro-controller, as it only needs 3V to energise and will take up to 32V. It can easily screw into any box it fits into

     

    Regards

     

    peter

     


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to Robert Peter Oakes

    Peter

    I agree that is a much better solution ...well done.

     

    I have heard that there are some solid state relays using  "... less than optimal parts ...." inside, so its is wise to run them at full load then remove the power and check if they get hot.

    The markings make them look like a genuine thing, but they are apparently a poor copy.

     

    The true test of any of these is the 1000v DC ( megger ) check between any of the Mains side and the low voltage control side and the metal mounting plate.

    For those interested element14 has these ( on special for NZ$122 ).

    image

     

    Mark