Arduino
  • Products
  • More
Arduino
Arduino Forum Using a Arduino in place of a DAQ
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 416 subscribers
  • Views 1238 views
  • Users 0 members are here
Related

Using a Arduino in place of a DAQ

e14 Contributor
e14 Contributor over 12 years ago

imageHi. I am new to electronics (very limited knowledge). I am trying to build a balancing machine to balance a small turbine. The circuit I have picks up signals from Piezo sensors and uses amplifiers that are coupled to a NI USG 6008 DAQ. This is a expensive unit (DAQ) Is it possible to use a Arduino in place of the DAQ? Will this be able to give me some form of readout/imaging on my PC as I would get with the DAQ?.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 12 years ago

    Hello Alfred, you're new to Data Acquisition if you think the NI 6008 is expensive - it's only £183 and from NI  (not the cheapest source in the world). You might just get away with an Arduino instead but the NI box is 12 bit resolution and the Arduino's Atmel Mega processor on board ADC is only 10 bits.

     

    What sort of turbine is it ?

     

    You might be able to get away with less effort by connecting the piezo sensors to the PC's audio inputs and using audio software to look at the signals.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelkellett

    Hi MK. Thank you for that. I have built a small jet turbine engine. The balancer is to balance the compressor, shaft and turbine wheel assembly.

    I have built a balancer that works with 4 piezo sensors with ? an analogue circuit. It does not seem to work well. there is a circuit available that uses the USB-6008 DAQ.

    I do however not want to spend so much money on the DAQ. The DAQ software does however give a very good image setup on the computer that would make balancing more accurate, as it indicates where the area of imbalance is. How would I be connecting the piezo sensors to the PC`s audio inputs?

     

    Alfred

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    What type of piezo sensor do you have, and what is the rpm at which you will balance. The PC will probably only have two audio inputs so it may not do for this. Why do you need 4 sensors, wheel balancers only use two, there are references on the web for doing it with 2 sensors.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    What type of piezo sensor do you have, and what is the rpm at which you will balance. The PC will probably only have two audio inputs so it may not do for this. Why do you need 4 sensors, wheel balancers only use two, there are references on the web for doing it with 2 sensors.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelkellett

    The balancer is constructed with 2 T-shaped structures with a piezo sensor (flat disc type) on arm. I got this from the Gas turbine association web.The shaft with its compressor and turbine wheel is put on top of this and rotated at not more than 5000rpm.The 4 piezos probably help in working out where the imbalance on the shaft and components are. This triggers a LED that shows a spot on the turbine. I know there are balancers with only 2 piezos, but they are constructed different. I can combine the 2 sensors on each T-structure if need be. At the moment I switch between the 4 sensors and view the signal on a analogue meter. The weaker the signal indicates that it is in balance. I am however finding it is not very sensitive as the 2 piezos of each T give different signal strengths. The original circuit I am using now was upgraded to a more digital version, but this uses the DAQ to connect to the computer. I am sorry I cannot be very technical with the electronics as this is not my strong point.

    I do not know how to ad the circuit for you to view. This might make more sense to you.

     

    Alfred

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    It would make a lot more sense with a circuit - if you can get the schematic up on screen you can press the print screen key to get it on the clipboard, paste it into paint, save as a jpg and include it on E14 using the little camera icon 'paste image' button.

     

    If you are connecting piezo discs directly to a meter it won't work well.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelkellett

    Hi. I am sorry I do not know how the clipboard works,

    I have been able to attach them. Hope you can open the files.

     

    Alfred

    Attachments:
    imagemain - schematic.pdf
    imageDAQ Connection.pdf
    imagesensor schematic.pdf
    imageBalancer mechanical.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    Although there are 4 piezo sensors they are wired up in such a way that there are only two channels of analogue data. Your problem is that the original designer of this system has out quite a lot of effort into it and I suspect has done a fair bit of work on the software. Although you could certainly use an Arduino in place of the NI DAQ you would need to modify the software quite significantly. Unless you are experienced in this sort of work it will take you a very long time.

    Why not ask the original designer if they have any plans to port their code to an Arduino (or some other  very low cost hardware).

    The only problem with using  a sound card with the sensors is that you really need a third input for the optical sensor.

     

    I'm sorry but the only way round using the NI DAQ will require a lot of redesign work.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelkellett

    Thanks a lot for going through all this for me. I probably would be better of getting the DAQ.

    I shall shop around for a good price.

     

    Alfred