Arduino
  • Products
  • More
Arduino
Arduino Forum AC power meter not using RMS of a sine wave
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 416 subscribers
  • Views 289 views
  • Users 0 members are here
  • rms
  • ac
  • wattmeter
Related

AC power meter not using RMS of a sine wave

e14 Contributor
e14 Contributor over 12 years ago

Hello I hope someone can help me. I am new to the Arduino environment. I have just completed a build of a 3D printer made by SeeMeCNC called Rostock MAX V2.0/ It uses the Auduino environment so I have used the system type a little bit. I am impressed by the Arduino system and support. My needs now are not related to the 3D printer.

 

I want to make a module to calculate the true power delivered to a heater not the apparent power. The controller utilizes a triac output device so I am not dealing with a sine wave system. I have two outputs from the controller that I have built, one for voltage delivered to the heating element and one that represents the current delivered.

 

The voltage output is  from a 100 to 1 voltage divider since the heater is running on 240vac I should see a signal from 0 to 5V max bipolar. I know that the Arduino has unipolar inputs so I will be putting a level shifting network and capacitively couple the output to be unipolar to the 0 to 5V range. i.e. 2.5 volts would equal 0 volts.

 

The current output is derived from an toroidal core inductor that has the power lead to the load passing through the core. I get about 3Vac rms for a 30 amp load. Measured using a sine wave source (triac not in system). Again I will couple my AC sense with a capacitor to a level shifting network to satisfy the unipolar inputs and to maintain phase angle for the power calculations.

 

What I need to do is read these two signals at about 256 times the AC fundamental of 60Hz (16ms/256) produce a product that represents the power, then display this result on a LCD display. I do not know if this platform will handle the speed needed. Is there anyone that knows the platform that could recommend the products needed?

 

I have ability to program in C if needed. Maybe someone has already done this and I could be pointed in the right direction. I will develop the skills needed if this platform will yield results. I just want to have an idea that this platform will handle the developed results.

  • Sign in to reply
  • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    Try a look at the tiva c series connected launch pads , these have 12  hardware ADC channels at 12bit and they can run autonomously at up-to  2M samples per second as well as do averaging etc if needed

     

    cpu runs at 120Mhz so is more than fast enough

     

    you also program it in c

     

    it includes an Ethernet port and a wealth of other io options

     

    you can buy one for under 30$