Arduino
  • Products
  • More
Arduino
Arduino Forum Temperature-control with arduino / MAX31855 / NXP KTY84
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 2742 views
  • Users 0 members are here
  • temperature
  • maxim
  • nxp
  • arduino
  • sensor
Related

Temperature-control with arduino / MAX31855 / NXP KTY84

e14 Contributor
e14 Contributor over 12 years ago

Hello Community,

 

I'm a software engineer  so I don't have much experience with HW. My goal is to create a small temperature-control with an arduino and I already found some parts that might work together, but I'm not sure about that and it would be great  if someone more experienced could help me out.

 

Basically I want to measure temperatures up to about 200-250 °C that are created by a e-cigarette-heating element. If the temperature exceeds a certain limit, I want to turn off the heating element. If the temperature drops below a threshold I want to turn the heating element back on.

The control is done by an arduino UNO. Because the heating element needs a lot of power (well not THAT much, but propably more than the arduino can handle), I would use a MOSFET controlled by the arduino to switch it on and off.

 

The measurement could be done using a MAX31855 (Type K) connected via SPI to the arduino. As a thermocoupler I would use a NXP KTY84 which has a tempeture-range from -40°C to +300°C which should be good.

 

So here are the questions:

- Will a MAX31855 work with the NXP KTY84? (I think so, because it has a K in its label. image )

- What kind of MOSFET do you recommend? (I have no idea, but is needs to be activated with the 5V of the Arduino.

 

 

Here are some links to datasheets. They are also attached to this topic:

MAX31855: https://www.adafruit.com/datasheets/MAX31855.pdf

NXP KTY84: http://www.produktinfo.conrad.com/datenblaetter/175000-199999/183458-da-01-en-Temperatursensor_KTY84.pdf

Thanks in advance for your help!

 

Marc

Attachments:
image183458-da-01-en-Temperatursensor_KTY84.pdf
imageMAX31855.pdf
  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 12 years ago

    Hi Marc,

     

    The NXP device is not a thermocouple, according to the datasheet it's resistance varies with temperature. A thermocouple generates a voltage with temperature. So the MAX.. device is not compatible. The resistance of the NXP device could be measured using a constant current source and an ADC. I've not done the math to know if the ADC on an Arduino is sufficient for your needs, you'd need to go through the NXP data sheet and the data sheet for your ADC. You probably need to enlist the help of a hardware engineer at this stage though, I don't think a prototype for such a solution can be constructed just from existing Arduino shields.

     

    Maybe a bi-metallic strip is an alternative idea? I know nothing about them though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 12 years ago

    Hi Marc,

     

    The NXP device is not a thermocouple, according to the datasheet it's resistance varies with temperature. A thermocouple generates a voltage with temperature. So the MAX.. device is not compatible. The resistance of the NXP device could be measured using a constant current source and an ADC. I've not done the math to know if the ADC on an Arduino is sufficient for your needs, you'd need to go through the NXP data sheet and the data sheet for your ADC. You probably need to enlist the help of a hardware engineer at this stage though, I don't think a prototype for such a solution can be constructed just from existing Arduino shields.

     

    Maybe a bi-metallic strip is an alternative idea? I know nothing about them though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    I feel really stupid right now, for not recognizing that the NXP is not a thermocouple...image Thx for the info!