Arduino
  • Products
  • More
Arduino
Arduino Forum 5V on ADC that is set to a reference of 3.3V? What happens?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 418 subscribers
  • Views 5175 views
  • Users 0 members are here
  • aref
  • analogreference
  • arduino
Related

5V on ADC that is set to a reference of 3.3V? What happens?

e14 Contributor
e14 Contributor over 12 years ago

Hi,

 

Normally you can put up to 5V to the analog-pins. Let's say you set your reference to 3.3V by connecting the 3.3V to the AREF-pin and call analogReference(EXTERNAL).

 

What happens now if you put 5V to the pin? Will it still put out 1024 as MAX-value or will it burn the arduino?

 

Background:

I have a thermal sensor that has a range from 500 to about 1700 Ohm for a temperature range from 0°C to 200°C. Combined with a 1kOhm resistor I want to use this as a voltage divider for the analog-in. With these settings the voltage will be between 1.6V and 3.15V, so i can't use the full range of the ADC but by setting the reference voltage to 3.3V I can increase the useable area from about 30% to 50% which gives me a better temperature resolution (0.4°C/step instead of 0.6°C).

 

BUT when the temperature increases above 235°C the input voltage will increase over 3.3V!

 

Thx in advance for your answers!

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 12 years ago


    Hi Marc - You are correct. Any voltage above the 3.3 volts will not harm the Arduino but all values will return a 1023. Here is a link to Arduino home that covers this.

     

    http://forum.arduino.cc/index.php/topic,119109.0.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to jw0752

    Ok, sounds good for my needs. I will just treat values above 1020 as dangerous and switch the heating element of.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to jw0752

    Ok, sounds good for my needs. I will just treat values above 1020 as dangerous and switch the heating element of.