Arduino Forum Arduino programming HELP NEEDED!!!
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
  • State Not Answered
  • Replies 44 replies
  • Subscribers 403 subscribers
  • Views 3153 views
  • Users 0 members are here
  • programming
  • rtc
  • code
  • arduino
  • relay
Related

Arduino programming HELP NEEDED!!!

Former Member
Former Member over 11 years ago

Hello! I am currently working on a project that requires a relay to be switched on at a certain time using a TinyRTC module. I understand that this should be fairly simple... but I can't get the code to play out correctly. Could someone PLEASE help me?

  • Sign in to reply
  • Cancel
Parents
  • kidiccurus
    0 kidiccurus over 11 years ago

    Can you please post your currant code and circuit diagram. Also, if it is literally just switching something on at a certain time, you may be better off with one of these:

    http://www.amazon.co.uk/Electronic-digital-mains-Socket-Display/dp/B002P7RF9A/ref=sr_1_1?ie=UTF8&qid=1408837264&sr=8-1&keywords=plug+timer

    I use and old mechanical version to automatically switch off my soldering iron every 20 minutes so I cant leave it on overnight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kidiccurus

    I don't really have any code yet. Everything I have started on is a bust. I am building a school bell timer to ring before and in-between classes. I have an arduino uno, a sainsmart 2-channel relay module, and a tinyrtc ic2. Currently the bell is operated by a button wich closes the connection between two wires. All I need to do is tell the arduino to switch the relay and close the connection for 'x' amount of time (about 2 seconds) at certain times throughout the day.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to kidiccurus

    And this will be your actual code. Well almost. Read the comments (grey stuff) they explain how to correctly set it up. I needed about a minute after I saw your post to finish it but I uploaded the other code first so you didn't need to wait.

    //Bellclock v1.0 Created by kidiccurus I alow you to use this program on the condition that no more than 1 (one) Great British Pound (GB£) of revenue will be generated as a result of its use or sale. Just put that in there to stop you selling this to anyone
    //Conect your relay to digital pin 4
    //requires the libary you just installed
     
    #include <Wire.h>
    #include "RTClib.h"
    //Please est the lenght of time (in seconds) you would like the bell to ring for here in place of the number 2. Please do not set a decimal.
    int belltime = 2;
    int relay = 4;
    RTC_DS1307 RTC;
    void setup() {
      Wire.begin();
       RTC.begin();
       pinMode(relay,OUTPUT);
    }
    void loop() {
      
     //This module rings the bell. In the top row, the number 12 can be changed for the hour in 24 hour format and the number 0 can be changed for the minute (0-59).
     //Please copy and paste this module as many times as required 
      if (now.hour() == 12 && now.minute() == 0){
        digitalWrite(relay,HIGH);
        delay(belltime*1000);
        digitalWrite(relay,LOW);
         };
     //This is the end of the module if you are going to copy and paste
      
     //Place here
    //Or here
    //Or here 
      
    //Or here  
      
    //Or here
    
    //Et cetera et cetera
      
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to kidiccurus

    Just spotted a minor glitch. After the line "digitalWrite(relay,LOW); " In theBell ringing module,please add the line "delay(59000);" Whithout this the code will ring the bell for a full minute.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kidiccurus

    On this first bit of code (for setting the clock), I have verified that my computer time is correct, but when I upload to the arduino, the time is not the same and is incorrect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Nevermind! I got the time set correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to Former Member

    Great. Now make sure you update the code according to instructions. It would be embarrassing for my code to annoy the large amount of people who will be within range of the bell when it goes off. Any other requests for the code please don't hesitate to post here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kidiccurus

    Thank you for the code! I have one more request. I don't want to mess up the formatting in the code, so could you post it again with 10 bell timing modules? (10 different times to ring the bell)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to Former Member

    Here you go. One little request from me. I you put this in a case, please could you write the number 42 on the inside, Just as a fun little hitchhikers reference.

    //Bellclock v1.0 Created by kidiccurus I alow you to use this program on the condition that no more than 1 (one) Great British Pound (GB£) of revenue will be generated as a result of its use or sale. Just put that in there to stop you selling this to anyone
    //Conect your relay to digital pin 4
    //requires the libary you just installed
     
    #include <Wire.h>
    #include "RTClib.h"
    //Please est the lenght of time (in seconds) you would like the bell to ring for here in place of the number 2. Please do not set a decimal.
    int belltime = 2;
    int relay = 4;
    RTC_DS1307 RTC;
    void setup() {
      Wire.begin();
       RTC.begin();
       pinMode(relay,OUTPUT);
    }
    void loop() {
      
     //This module rings the bell. In the top row, the number 12 can be changed for the hour in 24 hour format and the number 0 can be changed for the minute (0-59).
     //Please copy and paste this module as many times as required 
      if (now.hour() == 12 && now.minute() == 0){
        digitalWrite(relay,HIGH);
        delay(belltime*1000);
        digitalWrite(relay,LOW);
        delay(59000);
         };
     //This is the end of the module if you are going to copy and paste
      
     //This module rings the bell. In the top row, the number 12 can be changed for the hour in 24 hour format and the number 0 can be changed for the minute (0-59).
     //Please copy and paste this module as many times as required 
      if (now.hour() == 12 && now.minute() == 0){
        digitalWrite(relay,HIGH);
        delay(belltime*1000);
        digitalWrite(relay,LOW);
        delay(59000);
         };
     //This is the end of the module if you are going to copy and paste
      
     //This module rings the bell. In the top row, the number 12 can be changed for the hour in 24 hour format and the number 0 can be changed for the minute (0-59).
     //Please copy and paste this module as many times as required 
      if (now.hour() == 12 && now.minute() == 0){
        digitalWrite(relay,HIGH);
        delay(belltime*1000);
        digitalWrite(relay,LOW);
        delay(59000);
         };
     //This is the end of the module if you are going to copy and paste
      
     //This module rings the bell. In the top row, the number 12 can be changed for the hour in 24 hour format and the number 0 can be changed for the minute (0-59).
     //Please copy and paste this module as many times as required 
      if (now.hour() == 12 && now.minute() == 0){
        digitalWrite(relay,HIGH);
        delay(belltime*1000);
        digitalWrite(relay,LOW);
        delay(59000);
         };
     //This is the end of the module if you are going to copy and paste
      
      
     //This module rings the bell. In the top row, the number 12 can be changed for the hour in 24 hour format and the number 0 can be changed for the minute (0-59).
     //Please copy and paste this module as many times as required 
      if (now.hour() == 12 && now.minute() == 0){
        digitalWrite(relay,HIGH);
        delay(belltime*1000);
        digitalWrite(relay,LOW);
        delay(59000);
         };
     //This is the end of the module if you are going to copy and paste
      
      
     //This module rings the bell. In the top row, the number 12 can be changed for the hour in 24 hour format and the number 0 can be changed for the minute (0-59).
     //Please copy and paste this module as many times as required 
      if (now.hour() == 12 && now.minute() == 0){
        digitalWrite(relay,HIGH);
        delay(belltime*1000);
        digitalWrite(relay,LOW);
        delay(59000);
         };
     //This is the end of the module if you are going to copy and paste
      
     //This module rings the bell. In the top row, the number 12 can be changed for the hour in 24 hour format and the number 0 can be changed for the minute (0-59).
     //Please copy and paste this module as many times as required 
      if (now.hour() == 12 && now.minute() == 0){
        digitalWrite(relay,HIGH);
        delay(belltime*1000);
        digitalWrite(relay,LOW);
        delay(59000);
         };
     //This is the end of the module if you are going to copy and paste
     
      //This module rings the bell. In the top row, the number 12 can be changed for the hour in 24 hour format and the number 0 can be changed for the minute (0-59).
     //Please copy and paste this module as many times as required 
      if (now.hour() == 12 && now.minute() == 0){
        digitalWrite(relay,HIGH);
        delay(belltime*1000);
        digitalWrite(relay,LOW);
        delay(59000);
         };
     //This is the end of the module if you are going to copy and paste
      
      //This module rings the bell. In the top row, the number 12 can be changed for the hour in 24 hour format and the number 0 can be changed for the minute (0-59).
     //Please copy and paste this module as many times as required 
      if (now.hour() == 12 && now.minute() == 0){
        digitalWrite(relay,HIGH);
        delay(belltime*1000);
        digitalWrite(relay,LOW);
        delay(59000);
         };
     //This is the end of the module if you are going to copy and paste
      
      //This module rings the bell. In the top row, the number 12 can be changed for the hour in 24 hour format and the number 0 can be changed for the minute (0-59).
     //Please copy and paste this module as many times as required 
      if (now.hour() == 12 && now.minute() == 0){
        digitalWrite(relay,HIGH);
        delay(belltime*1000);
        digitalWrite(relay,LOW);
        delay(59000);
         };
     //This is the end of the module if you are going to copy and paste
         
      
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kidiccurus

    Yes I can do that image Thank you again!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to Former Member

    Your welcome. Please make sure you test it. It is simple code but I don't want to make any large mistakes. Also, could you please mark my answer as correct so people know that you don't need any more help. Where is this going to be installed? It would be nice to know who I have helped plus it could could be good for a resume in the future.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kidiccurus

    I thought I got the time set, but it isn't wanting to work. It isnt setting the time from my computer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to kidiccurus

    I thought I got the time set, but it isn't wanting to work. It isnt setting the time from my computer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to Former Member

    // Date and time functions using a DS1307 RTC connected via I2C and Wire lib
    
    #include <Wire.h>
    #include "RTClib.h"
    
    RTC_DS1307 RTC;
    
    void setup () {
        Serial.begin(57600);
        Wire.begin();
        RTC.begin();
    
    rtc.adjust(DateTime(2014,MONTH,DAY,HOUR,MINUTE,0));
      }
    
    }
    
    void loop () {
    
    }

    Right, try this. Line 13, replace the month day hour and minute with the correct numerical values.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kidiccurus

    Im getting these errors when I try to upload


    Untitled_Project.ino:13:1: error: use of undeclared identifier 'rtc'

    rtc.adjust(DateTime(2014,8,23,21,18,0));

    ^
    Untitled_Project.ino:16:1: error: extraneous closing brace ('}')

    }

    ^

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to Former Member

    Change rtc to RTC (block capitals)
    and delete the curly brace directly underneath it. It is quite late where I am at the moment so I am making a few silly mistakes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kidiccurus

    I got the time set, but when I upload the bellring sketch I get this


    BellRing.ino:19:7: error: use of undeclared identifier 'now'

      if (now.hour() == 21 && now.minute() == 26){

      ^
    BellRing.ino:19:27: error: use of undeclared identifier 'now'

      if (now.hour() == 21 && now.minute() == 26){

      ^
    2 errors generated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to Former Member

    Add this line directly above the first bellring module. (line 17): DateTime now = RTC.now();

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kidiccurus

    Okay. That worked. Also I forgot to mention that my relay module works different than most others. It switches OFF when power is supplied to the control pin. To fix that I would just have to switch the 'HIGH' and 'LOW' in your code, correct?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to Former Member

    Yep, that is correct. I also recommend that you add the line "digitalWrite(relay,HIGH);"  between line 14 and 15. Without this the bell will ring non stop until the first alarm as the pin defaults as low. An active low relay seems quite dangerous to me. Here, if the control circuitry fails the bell will ring constantly, and in an oven this could start a fire. I recommend you add a suitable switch to override the relay to spare everyone's ears if it does go wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kidiccurus

    I just tested it out but it was delayed by about a minute and the relay stayed on for almost two minutes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to Former Member

    how long did you set the relay to go on for what number did you actually enter. As for the delay, your time may be a minute or so behind from when you where uploading the time. It probably took about a minute for the rtc to be programed with the time from when you entered it in the time setting program. Try setting the time a minute in the future when using the upload program to help compensate.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to kidiccurus

    I set the belltiime as "2" and then changed the "(belltime*1000)" to just "(2000)" but it still does the same thing