Arduino
  • Products
  • More
Arduino
Arduino Forum Is it possible to avoid using 3rd pin on 3 pin IR detector?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 1676 views
  • Users 0 members are here
  • infrared
  • wiring
  • sensor
Related

Is it possible to avoid using 3rd pin on 3 pin IR detector?

e14 Contributor
e14 Contributor over 12 years ago

I've been looking around for IR detectors and i only seemed to come across 3-pin diodes; i would feel much comfortable wiring is there was only 2 pins. so is there a way i can avoid wiring the ground pin or can someone direct me to a site where i could purchase 2-pin IR photodiodes that are roughly inexpensive i need 189 of them.

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    The reason there are three pins is because two are for power, one is for data

     

    with IR remote receiver devices (Which your probably finding in your search) like these the device does more than a simple IR detection, many have a built in 38Khz decoder to save you having to deal with it, it output the native IR Remote codes less the carrier frequency

     

    either way, two pins are for power and one data, so you can not easily get rid of one pin. If you replaced it with a true and simple IR Photo resistor or  transistor then u could get rid of a pin but you may need additional circuitry or code

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    The reason there are three pins is because two are for power, one is for data

     

    with IR remote receiver devices (Which your probably finding in your search) like these the device does more than a simple IR detection, many have a built in 38Khz decoder to save you having to deal with it, it output the native IR Remote codes less the carrier frequency

     

    either way, two pins are for power and one data, so you can not easily get rid of one pin. If you replaced it with a true and simple IR Photo resistor or  transistor then u could get rid of a pin but you may need additional circuitry or code

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    OOh okay thanks a lot. I don't know if it helps but I was placing IR emitters around them and if the light is reflected and picked by the detectors then it'll turn on surrounding visible light LEDs.