Arduino
  • Products
  • More
Arduino
Arduino Forum Is it possible to avoid using 3rd pin on 3 pin IR detector?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 1676 views
  • Users 0 members are here
  • infrared
  • wiring
  • sensor
Related

Is it possible to avoid using 3rd pin on 3 pin IR detector?

e14 Contributor
e14 Contributor over 12 years ago

I've been looking around for IR detectors and i only seemed to come across 3-pin diodes; i would feel much comfortable wiring is there was only 2 pins. so is there a way i can avoid wiring the ground pin or can someone direct me to a site where i could purchase 2-pin IR photodiodes that are roughly inexpensive i need 189 of them.

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 12 years ago

    2 pin photodiodes will need an amplifier to make their signal useful, which could end up to be a lot of circuitry.

    3 pin semiconductor light sensors can have amplification built-in, but the price is higher as well as having more pins.

    2 pin phototransistors are probably better for your application and may cost about 8 cents each.

    2 pin photodarlingtons are even more sensitive and probably best for your application and may cost about 30 cents each.

    2 pin CdS sensors cost less than 6 cents each, but need an external transistor to control other LEDs and they start to lose sensitivity at IR wavelengths.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dougw

    Thanks alot that was very helpful. What's the difference between a phototransitor and a photodarlington? With the photodiodes i was planning to use a TLC274 Op-Amp

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dougw

    Thanks alot that was very helpful. What's the difference between a phototransitor and a photodarlington? With the photodiodes i was planning to use a TLC274 Op-Amp

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dougw
    0 dougw over 12 years ago in reply to e14 Contributor

    A photodarlington doesn't need any op-amps - it can drive LEDs directly. Photdarlingtons are simply 2 phototransistors in a darlington configuration which makes them about 100 times more sensitive than phototransistors. It is easy to block some of the light with tape if they are too sensitive.