Arduino Forum Arduino LCD 20x4 I2C problem
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
  • State Suggested Answer
  • Replies 17 replies
  • Answers 2 answers
  • Subscribers 403 subscribers
  • Views 3529 views
  • Users 0 members are here
  • i2c
  • 20x4
  • led
  • arduino
Related

Arduino LCD 20x4 I2C problem

Former Member
Former Member over 11 years ago

Hi

 

I have some problem with geting my code to work after a changed my LCD from a 16x2 to a 20x4 with I2C inteface.

 

If i try the sample code below the new LCD works:

 

#include <Wire.h>
#include <LCD.h>
#include <LiquidCrystal_I2C.h>

#define I2C_ADDR    0x3F
#define BACKLIGHT_PIN     3
#define En_pin  2
#define Rw_pin  1
#define Rs_pin  0
#define D4_pin  4
#define D5_pin  5
#define D6_pin  6
#define D7_pin  7

int n = 1;

LiquidCrystal_I2C        lcd(I2C_ADDR,En_pin,Rw_pin,Rs_pin,D4_pin,D5_pin,D6_pin,D7_pin);

void setup()
{
lcd.begin (20,4); // <<----- My LCD was 16x2

 
// Switch on the backlight
lcd.setBacklightPin(BACKLIGHT_PIN,POSITIVE);
lcd.setBacklight(HIGH);
lcd.home (); // go home

lcd.print("SainSmartI2C16x2");
}

void loop()
{
// Backlight on/off every 3 seconds
lcd.setCursor (0,1);        // go to start of 2nd line
lcd.print(n++,DEC);
lcd.setBacklight(LOW);      // Backlight off
delay(3000);
lcd.setBacklight(HIGH);     // Backlight on
delay(3000);
}

 

 

But when I try to do it with my own code I just got 2 rows with "#"

 

I use this library:

LiquidCrystal_V1.2.1 - https://bitbucket.org/fmalpartida/new-liquidcrystal/downloads

MenuBackEnd V1.4 - http://www.arduino.cc/playground/uploads/Profiles/MenuBackend_1-4.zip

 

 

Here is my code that I can't get to work.

#include <Wire.h>
#include <LCD.h>
#include <LiquidCrystal_I2C.h>
#include <MenuBackend.h>


#define I2C_ADDR    0x3F
#define BACKLIGHT_PIN     3
#define En_pin  2
#define Rw_pin  1
#define Rs_pin  0
#define D4_pin  4
#define D5_pin  5
#define D6_pin  6
#define D7_pin  7


const int buttonPinLeft = 8;      // pin for the Up button
const int buttonPinRight = 9;    // pin for the Down button
const int buttonPinEsc = 10;     // pin for the Esc button
const int buttonPinEnter = 11;   // pin for the Enter button


int lastButtonPushed = 0;


int lastButtonEnterState = LOW;   // the previous reading from the Enter input pin
int lastButtonEscState = LOW;   // the previous reading from the Esc input pin
int lastButtonLeftState = LOW;   // the previous reading from the Left input pin
int lastButtonRightState = LOW;   // the previous reading from the Right input pin


long lastEnterDebounceTime = 0;  // the last time the output pin was toggled
long lastEscDebounceTime = 0;  // the last time the output pin was toggled
long lastLeftDebounceTime = 0;  // the last time the output pin was toggled
long lastRightDebounceTime = 0;  // the last time the output pin was toggled
long debounceDelay = 500;    // the debounce time


int Motor1=1;
int Motor2=0;
int Backlight=255;


String CWCCW, CWCCW2, TPD, TPD2;



LiquidCrystal_I2C lcd(I2C_ADDR,En_pin,Rw_pin,Rs_pin,D4_pin,D5_pin,D6_pin,D7_pin);




//Menu variables


MenuBackend menu = MenuBackend(menuUsed,menuChanged);


//initialize menuitems
    MenuItem Item1 = MenuItem("Item1"); //Motor 1 Settings


  MenuItem Item1Sub1 = MenuItem("Item1Sub1"); //TPD
  MenuItem Item1Sub1Sub1 = MenuItem("Item1Sub1Sub1"); //650
  MenuItem Item1Sub1Sub2 = MenuItem("Item1Sub1Sub2"); //750
  MenuItem Item1Sub1Sub3 = MenuItem("Item1Sub1Sub3"); //850
  MenuItem Item1Sub1Sub4 = MenuItem("Item1Sub1Sub4"); //950


  MenuItem Item1Sub2 = MenuItem("Item1Sub2");
  MenuItem Item1Sub2Sub1 = MenuItem("Item1Sub2Sub1"); //CW
  MenuItem Item1Sub2Sub2 = MenuItem("Item1Sub2Sub2"); //CCW
  MenuItem Item1Sub2Sub3 = MenuItem("Item1Sub2Sub3"); //Both
     
  MenuItem Item1Sub3 = MenuItem("Item1Sub3"); 
  MenuItem Item1Sub3Sub1 = MenuItem("Item1Sub3Sub1"); //Stop
  MenuItem Item1Sub3Sub2 = MenuItem("Item1Sub3Sub2"); //Start
     
  MenuItem Item2 = MenuItem("Item2"); //Motor 2 Settings

  MenuItem Item2Sub1 = MenuItem("Item2Sub1"); //TPD
  MenuItem Item2Sub1Sub1 = MenuItem("Item2Sub1Sub1"); //650
  MenuItem Item2Sub1Sub2 = MenuItem("Item2Sub1Sub2"); //750
  MenuItem Item2Sub1Sub3 = MenuItem("Item2Sub1Sub3"); //850
  MenuItem Item2Sub1Sub4 = MenuItem("Item2Sub1Sub4"); //950


  MenuItem Item2Sub2 = MenuItem("Item2Sub2");
  MenuItem Item2Sub2Sub1 = MenuItem("Item2Sub2Sub1"); //CW
  MenuItem Item2Sub2Sub2 = MenuItem("Item2Sub2Sub2"); //CCW
  MenuItem Item2Sub2Sub3 = MenuItem("Item2Sub2Sub3"); //Both
     
  MenuItem Item2Sub3 = MenuItem("Item2Sub3");
  MenuItem Item2Sub3Sub1 = MenuItem("Item2Sub3Sub1"); //Stop
  MenuItem Item2Sub3Sub2 = MenuItem("Item2Sub3Sub2"); //Start


  MenuItem Item3 = MenuItem("Item3"); //Backlight
  MenuItem Item3Sub1 = MenuItem("Item3Sub1"); //25%
  MenuItem Item3Sub2 = MenuItem("Item3Sub2"); //50%
  MenuItem Item3Sub3 = MenuItem("Item3Sub3"); //75%
  MenuItem Item3Sub4 = MenuItem("Item3Sub4"); //100%



void setup()
{
  lcd.begin (20,4); //  <<----- My LCD was 16x2
  // Switch on the backlight
  lcd.setBacklightPin(BACKLIGHT_PIN,POSITIVE);
  lcd.setBacklight(HIGH);
  lcd.home (); // go home
  lcd.print("SainSmart"); 


  CWCCW = String("Both");
  CWCCW2 = String(" CCW");
    TPD = String("650");
  TPD2 = String("850");

  pinMode(buttonPinLeft, INPUT);
  pinMode(buttonPinRight, INPUT);
  pinMode(buttonPinEnter, INPUT);
  pinMode(buttonPinEsc, INPUT);




  //configure menu
  menu.getRoot().add(Item1);

  Item1.addRight(Item2).addRight(Item3);

  Item1.add(Item1Sub1).addRight(Item1Sub2).addRight(Item1Sub3); //Motor 1 Settings
    Item1Sub1.add(Item1Sub1Sub1).addRight(Item1Sub1Sub2).addRight(Item1Sub1Sub3).addRight(Item1Sub1Sub4);
    Item1Sub2.add(Item1Sub2Sub1).addRight(Item1Sub2Sub2).addRight(Item1Sub2Sub3);
    Item1Sub3.add(Item1Sub3Sub1).addRight(Item1Sub3Sub2);


  Item2.add(Item2Sub1).addRight(Item2Sub2).addRight(Item2Sub3); //Motor 2 Settings
    Item2Sub1.add(Item2Sub1Sub1).addRight(Item2Sub1Sub2).addRight(Item2Sub1Sub3).addRight(Item2Sub1Sub4);
    Item2Sub2.add(Item2Sub2Sub1).addRight(Item2Sub2Sub2).addRight(Item2Sub2Sub3);
    Item2Sub3.add(Item2Sub3Sub1).addRight(Item2Sub3Sub2);

  Item3.add(Item3Sub1).addRight(Item3Sub2).addRight(Item3Sub3).addRight(Item3Sub4); //Backlight


  menu.toRoot();


}


void loop()
{
  readButtons();  //I splitted button reading and navigation in two procedures because
  navigateMenus();  //in some situations I want to use the button for other purpose (eg. to change some settings)
}




void menuChanged(MenuChangeEvent changed){


  MenuItem newMenuItem=changed.to; //get the destination menu


  if(newMenuItem.getName()==menu.getRoot()){
        lcd.setCursor(6,0);
        lcd.print("23:00:00");
        lcd.setCursor(5,1);
        lcd.print("2014/12/31");
  lcd.setCursor(0,2);
        lcd.print("                    ");
  lcd.setCursor(0,3);
        lcd.print("                    ");

  if (Motor1==1){
  lcd.setCursor(0,2); //set the start position for lcd printing to the second row
        lcd.print(TPD);
  lcd.setCursor(3,2);
  lcd.print("TPD");
  lcd.setCursor(0,3);
  lcd.print(CWCCW);
        } else if (Motor1==0){
          lcd.setCursor(0,2); //set the start position for lcd printing to the second row
          lcd.print("Not");
          lcd.setCursor(0,3);
   lcd.print("Active");
        }
       
  if (Motor2==1){
  lcd.setCursor(14,2); //set the start position for lcd printing to the second row
        lcd.print(TPD2);
  lcd.setCursor(17,2);
  lcd.print("TPD");
  lcd.setCursor(14,3);
  lcd.print(CWCCW2);
  } else if (Motor2==0){
          lcd.setCursor(17,2);
   lcd.print("Not");
   lcd.setCursor(14,3);
   lcd.print("Active");
   lcd.setCursor(0,2);
        lcd.print("test");
  
    }
  }
  else if(newMenuItem.getName()=="Item1"){ //Motor 1 Settings
  lcd.setCursor(0,3);
        lcd.print("                    ");
  lcd.setCursor(0,2);
        lcd.print("Motor 1 Settings    ");
  }
  else if(newMenuItem.getName()=="Item1Sub1"){ //M1 TPD
  lcd.setCursor(0,2);
        lcd.print("Motor 1 Settings    ");
  lcd.setCursor(0,3);
  lcd.print("TPD                 ");
  }
  else if(newMenuItem.getName()=="Item1Sub1Sub1"){ //650
  lcd.setCursor(0,2);
        lcd.print("Motor 1> TPD        ");
        if(TPD=="650"){
  lcd.setCursor(0,3);
  lcd.print("650 *               ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("650                 ");
  }
  }
  else if(newMenuItem.getName()=="Item1Sub1Sub2"){ //750
  lcd.setCursor(0,2);
    lcd.print("Motor 1> TPD        ");
  if(TPD=="750"){
  lcd.setCursor(0,3);
  lcd.print("750 *               ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("750                 ");
  }
  }
  else if(newMenuItem.getName()=="Item1Sub1Sub3"){ //850
  lcd.setCursor(0,2);
    lcd.print("Motor 1> TPD        ");
  if(TPD=="850"){
  lcd.setCursor(0,3);
  lcd.print("850 *               ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("850                 ");
  }
  }
  else if(newMenuItem.getName()=="Item1Sub1Sub4"){ //950
  lcd.setCursor(0,2);
    lcd.print("Motor 1> TPD        ");
  if(TPD=="950"){
  lcd.setCursor(0,3);
  lcd.print("950 *               ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("950                 ");
  }
  }
  else if(newMenuItem.getName()=="Item1Sub2"){ //M1 Driection
  lcd.setCursor(0,2);
    lcd.print("Motor 1 Settings    ");
  lcd.setCursor(0,3);
    lcd.print("Direction           ");
  }
  else if(newMenuItem.getName()=="Item1Sub2Sub1"){ //CW
  lcd.setCursor(0,2);
        lcd.print("Motor 1> Direrection");
  if(CWCCW=="CW"){
  lcd.setCursor(0,3);
  lcd.print("CW *                ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("CW                  ");
  }
  }
  else if(newMenuItem.getName()=="Item1Sub2Sub2"){ //CCW
  lcd.setCursor(0,2);
        lcd.print("Motor 1> Direrection");
  if(CWCCW=="CCW"){
  lcd.setCursor(0,3);
  lcd.print("CCW *               ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("CCW                 ");
  }
  }
  else if(newMenuItem.getName()=="Item1Sub2Sub3"){ //Both
  lcd.setCursor(0,2);
        lcd.print("Motor 1> Direrection");
  if(CWCCW=="CW/CCW"){
  lcd.setCursor(0,3);
  lcd.print("Both *              ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("Both                ");
  }
  }
  else if(newMenuItem.getName()=="Item1Sub3"){ // M1 START/STOP
  lcd.setCursor(0,2);
        lcd.print("Motor 1 Settings    ");
  lcd.setCursor(0,3);
  lcd.print("STOP/START          ");
  }
  else if(newMenuItem.getName()=="Item1Sub3Sub1"){
  lcd.setCursor(0,2);
        lcd.print("Motor 1> STOP/START ");
  lcd.setCursor(0,3);
  lcd.print("START               ");
  }
  else if(newMenuItem.getName()=="Item1Sub3Sub2"){
  lcd.setCursor(0,2);
        lcd.print("Motor 1> STOP/START ");
  lcd.setCursor(0,3);
  lcd.print("STOP                ");
  }
  else if(newMenuItem.getName()=="Item2"){ //Motor2 settings
  lcd.setCursor(0,3);
        lcd.print("                    ");
  lcd.setCursor(0,2);
        lcd.print("Motor 2 Settings    ");
  }
  else if(newMenuItem.getName()=="Item2Sub1"){ //M2 TPD
  lcd.setCursor(0,2);
    lcd.print("Motor 2 Settings    ");
  lcd.setCursor(0,3);
  lcd.print("TPD                 ");
  }
  else if(newMenuItem.getName()=="Item2Sub1Sub1"){ //650
        lcd.setCursor(0,2);
        lcd.print("Motor 2> TPD        ");
  if(TPD2=="650"){
  lcd.setCursor(0,3);
  lcd.print("650 *           ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("650             ");
  }
  }
  else if(newMenuItem.getName()=="Item2Sub1Sub2"){ //750
  lcd.setCursor(0,2);
    lcd.print("Motor 2> TPD        ");
  if(TPD2=="750"){
  lcd.setCursor(0,3);
  lcd.print("750 *               ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("750                 ");
  }
  }
  else if(newMenuItem.getName()=="Item2Sub1Sub3"){ //850
  lcd.setCursor(0,2);
        lcd.print("Motor 2> TPD        ");
  if(TPD2=="850"){
  lcd.setCursor(0,3);
  lcd.print("850 *               ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("850                 ");
  }
  }
  else if(newMenuItem.getName()=="Item2Sub1Sub4"){ //950
  lcd.setCursor(0,2);
        lcd.print("Motor 2> TPD        ");
  if(TPD=="950"){
  lcd.setCursor(0,3);
  lcd.print("950 *               ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("950                 ");
  }
  }
  else if(newMenuItem.getName()=="Item2Sub2"){ //M2 Direction
  lcd.setCursor(0,2);
        lcd.print("Motor 2> Direction  ");
  lcd.setCursor(0,3);
        lcd.print("Direction           ");
  }
  else if(newMenuItem.getName()=="Item2Sub2Sub1"){ //CW
  lcd.setCursor(0,2);
        lcd.print("Motor 2> Direction  ");
  if(CWCCW2=="    CW"){
  lcd.setCursor(0,3);
  lcd.print("CW *                ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("CW                  ");
  }
  }
  else if(newMenuItem.getName()=="Item2Sub2Sub2"){ //CCW
  lcd.setCursor(0,2);
    lcd.print("Motor 2> Direction  ");
  if(CWCCW2=="   CCW"){
  lcd.setCursor(0,3);
  lcd.print("CCW *               ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("CCW                 ");
  }
  }
  else if(newMenuItem.getName()=="Item2Sub2Sub3"){ //Both
  lcd.setCursor(0,2);
        lcd.print("Motor 2> Direction  ");
  if(CWCCW2=="CW/CCW"){
  lcd.setCursor(0,3);
  lcd.print("Both *              ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("Both                ");
  }
  }
  else if(newMenuItem.getName()=="Item2Sub3"){ // M2 START/STOP
  lcd.setCursor(0,2);
        lcd.print("Motor 2 Settings    ");
  lcd.setCursor(0,3);
  lcd.print("STOP/START          ");
  }
  else if(newMenuItem.getName()=="Item2Sub3Sub1"){
  lcd.setCursor(0,2);
        lcd.print("Motor 2> STOP/START ");
  lcd.setCursor(0,3);
  lcd.print("START               ");
  }
  else if(newMenuItem.getName()=="Item2Sub3Sub2"){
  lcd.setCursor(0,2);
        lcd.print("Motor 2> STOP/START ");
  lcd.setCursor(0,3);
  lcd.print("STOP                ");
  }
  else if(newMenuItem.getName()=="Item3"){ //backlight
  lcd.setCursor(0,3);
    lcd.print("                    ");
  lcd.setCursor(0,2);
    lcd.print("LCD Backlight       ");
  }
  else if(newMenuItem.getName()=="Item3Sub1"){ //25%
  lcd.setCursor(0,2);
    lcd.print("LCD Backlight       ");
  if(Backlight==64){
  lcd.setCursor(0,3);
  lcd.print("25% *               ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("25%                 ");
  }
  }
  else if(newMenuItem.getName()=="Item3Sub2"){ //50%
  lcd.setCursor(0,2);
    lcd.print("LCD Backlight       ");
  if(Backlight==128){
  lcd.setCursor(0,3);
  lcd.print("50% *               ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("50%                 ");
  }
  }
  else if(newMenuItem.getName()=="Item3Sub3"){ //75%
  lcd.setCursor(0,2);
    lcd.print("LCD Backlight       ");
  if(Backlight==192){
  lcd.setCursor(0,3);
  lcd.print("75% *               ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("75%                 ");
  }
  }
  else if(newMenuItem.getName()=="Item3Sub4"){ //100%
  lcd.setCursor(0,2);
    lcd.print("LCD Backlight       ");
  if(Backlight==255){
  lcd.setCursor(0,3);
  lcd.print("100% *              ");
  }else{
  lcd.setCursor(0,3);
  lcd.print("100%                ");
  }
  }
   
}


// här sätter man vad som ska hända efter man har valt något


void menuUsed(MenuUseEvent used){
  if(used.item=="Item1Sub1Sub1"){ //sätter TPD 650
  lcd.clear();
  TPD = String("650");
  lcd.setCursor(0,1);
  lcd.print("M1 TPD set to 650");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item1Sub1Sub2"){ //sätter TPD 750
  lcd.clear();
  TPD = String("750");
  lcd.setCursor(0,1);
  lcd.print("M1 TPD set to 750");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item1Sub1Sub3"){ //sätter TPD 850
  lcd.clear();
  TPD = String("850");
  lcd.setCursor(0,1);
  lcd.print("M1 TPD set to 850");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
        else if(used.item=="Item1Sub1Sub4"){ //sätter TPD 950
  lcd.clear();
  TPD = String("950");
  lcd.setCursor(0,1);
  lcd.print("M1 TPD set to 950");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item1Sub2Sub1"){ //sätter CW
  lcd.clear();
  CWCCW = String("CW");
  lcd.setCursor(0,1);
  lcd.print("M1 Direction = CW");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item1Sub2Sub2"){ //sätter CCW
  lcd.clear();
  CWCCW = String("CCW");
  lcd.setCursor(0,1);
  lcd.print("M1 Direction = CCW");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item1Sub2Sub3"){ //sätter CW&CCW
  lcd.clear();
  CWCCW = String("CW/CCW");
  //turnmode = 0;
  lcd.setCursor(0,1);
  lcd.print("M1 Direction = Both");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item1Sub3Sub1"){ //Startar M1
  lcd.clear();
  lcd.setCursor(0,1);
                Motor1=1;
  lcd.print("Start Motor 1   ");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item1Sub3Sub2"){ //Stoppar M1
  lcd.clear();
  lcd.setCursor(0,1);
                Motor1=0;
  lcd.print("Stop Motor 1    ");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item2Sub1Sub1"){ //sätter TPD 650
  lcd.clear();
  TPD2 = String("650");
  lcd.setCursor(0,1);
  lcd.print("M2 TPD set to 650");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item2Sub1Sub2"){ //sätter TPD 750
  lcd.clear();
  TPD2 = String("750");
  lcd.setCursor(0,1);
  lcd.print("M2 TPD set to 750");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item2Sub1Sub3"){ //sätter TPD 850
  lcd.clear();
  TPD2 = String("850");
  lcd.setCursor(0,1);
  lcd.print("M2 TPD set to 850");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
    else if(used.item=="Item2Sub1Sub4"){ //sätter TPD 950
  lcd.clear();
  TPD2 = String("950");
  lcd.setCursor(0,1);
  lcd.print("M2 TPD set to 950");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item2Sub2Sub1"){ //sätter CW
  lcd.clear();
  CWCCW2 = String("    CW");
  lcd.setCursor(0,1);
  lcd.print("M2 Direction = CW");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item2Sub2Sub2"){ //sätter CCW
  lcd.clear();
  CWCCW2 = String("   CCW");
  lcd.setCursor(0,1);
  lcd.print("M2 Direction = CCW");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item2Sub2Sub3"){ //sätter CW&CCW
  lcd.clear();
  CWCCW2 = String("CW/CCW");
  lcd.setCursor(0,1);
  lcd.print("M2 Direction = Both");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item2Sub3Sub1"){ //Startar M1
  lcd.clear();
  lcd.setCursor(0,1);
                Motor2=1;
  lcd.print("Start Motor 2   ");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item2Sub3Sub2"){ //Stoppar M1
  lcd.clear();
  lcd.setCursor(0,1);
                Motor2=0;
  lcd.print("Stop Motor 2   ");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item3Sub1"){ //Blacklight 25%
  lcd.clear();
  Backlight=64;
  lcd.setBacklight(64);
  lcd.setCursor(0,1);
  lcd.print("Backlight = 25% ");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item3Sub2"){ //Blacklight 50%
  lcd.clear();
  Backlight=128;
  lcd.setBacklight(128);
  lcd.setCursor(0,1);
  lcd.print("Backlight = 50% ");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item3Sub3"){ //Blacklight 75%
  lcd.clear();
  Backlight=192;
  lcd.setBacklight(192);
  lcd.setCursor(0,1);
  lcd.print("Backlight = 75% ");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }
  else if(used.item=="Item3Sub4"){ //Blacklight 100%
  lcd.clear();
  Backlight=255;
  lcd.setBacklight(255);
  lcd.setCursor(0,1);
  lcd.print("Backlight = 100%");
  delay(3000);  //delay to allow message reading
  lcd.clear();
  menu.toRoot();  //back to Main
  }

}


void  readButtons(){  //read buttons status


  int reading;
  int buttonEnterState=LOW;             // the current reading from the Enter input pin
  int buttonEscState=LOW;             // the current reading from the input pin
  int buttonLeftState=LOW;             // the current reading from the input pin
  int buttonRightState=LOW;             // the current reading from the input pin


  //Enter button
                  // read the state of the switch into a local variable:
                  reading = digitalRead(buttonPinEnter);
                  // check to see if you just pressed the enter button
                  // (i.e. the input went from LOW to HIGH),  and you've waited
                  // long enough since the last press to ignore any noise:
                  // If the switch changed, due to noise or pressing:
                  if (reading != lastButtonEnterState) {
                    // reset the debouncing timer
                    lastEnterDebounceTime = millis();
                  }
                  if ((millis() - lastEnterDebounceTime) > debounceDelay) {
                    // whatever the reading is at, it's been there for longer
                    // than the debounce delay, so take it as the actual current state:
                    buttonEnterState=reading;
                    lastEnterDebounceTime=millis();
                  }
                  // save the reading.  Next time through the loop,
                  // it'll be the lastButtonState:
                  lastButtonEnterState = reading;


    //Esc button
                  // read the state of the switch into a local variable:
                  reading = digitalRead(buttonPinEsc);
                  // check to see if you just pressed the Down button
                  // (i.e. the input went from LOW to HIGH),  and you've waited
                  // long enough since the last press to ignore any noise:
                  // If the switch changed, due to noise or pressing:
                  if (reading != lastButtonEscState) {
                    // reset the debouncing timer
                    lastEscDebounceTime = millis();
                  }
                  if ((millis() - lastEscDebounceTime) > debounceDelay) {
                    // whatever the reading is at, it's been there for longer
                    // than the debounce delay, so take it as the actual current state:
                    buttonEscState = reading;
                    lastEscDebounceTime=millis();
                  }
                  // save the reading.  Next time through the loop,
                  // it'll be the lastButtonState:
                  lastButtonEscState = reading;
   //Down button
                  // read the state of the switch into a local variable:
                  reading = digitalRead(buttonPinRight);
                  // check to see if you just pressed the Down button
                  // (i.e. the input went from LOW to HIGH),  and you've waited
                  // long enough since the last press to ignore any noise:
                  // If the switch changed, due to noise or pressing:
                  if (reading != lastButtonRightState) {
                    // reset the debouncing timer
                    lastRightDebounceTime = millis();
                  }
                  if ((millis() - lastRightDebounceTime) > debounceDelay) {
                    // whatever the reading is at, it's been there for longer
                    // than the debounce delay, so take it as the actual current state:
                    buttonRightState = reading;
  lastRightDebounceTime =millis();
                  }
                  // save the reading.  Next time through the loop,
                  // it'll be the lastButtonState:
                  lastButtonRightState = reading;
    //Up button
                  // read the state of the switch into a local variable:
                  reading = digitalRead(buttonPinLeft);
                  // check to see if you just pressed the Down button
                  // (i.e. the input went from LOW to HIGH),  and you've waited
                  // long enough since the last press to ignore any noise:
                  // If the switch changed, due to noise or pressing:
                  if (reading != lastButtonLeftState) {
                    // reset the debouncing timer
                    lastLeftDebounceTime = millis();
                  }
                  if ((millis() - lastLeftDebounceTime) > debounceDelay) {
                    // whatever the reading is at, it's been there for longer
                    // than the debounce delay, so take it as the actual current state:
                    buttonLeftState = reading;
                    lastLeftDebounceTime=millis();;
                  }
                  // save the reading.  Next time through the loop,
                  // it'll be the lastButtonState:
                  lastButtonLeftState = reading;
                  //records which button has been pressed
                  if (buttonEnterState==HIGH){
                    lastButtonPushed=buttonPinEnter;
                  }else if(buttonEscState==HIGH){
                    lastButtonPushed=buttonPinEsc;
                  }else if(buttonRightState==HIGH){
                    lastButtonPushed=buttonPinRight;
                  }else if(buttonLeftState==HIGH){
                    lastButtonPushed=buttonPinLeft;
                  }else{
     lastButtonPushed=0;
                  }
}


void navigateMenus() {
  MenuItem currentMenu=menu.getCurrent();
  switch (lastButtonPushed){
  case buttonPinEnter:
  if(!(currentMenu.moveDown())){  //if the current menu has a child and has been pressed enter then menu navigate to item below
  menu.use();
  }else{  //otherwise, if menu has no child and has been pressed enter the current menu is used
  menu.moveDown();
  }
  break;
  case buttonPinEsc:
  menu.toRoot();  //back to main
  break;
  case buttonPinRight:
  menu.moveRight();
  break;
  case buttonPinLeft:
  menu.moveLeft();
  break;
  }
  lastButtonPushed=0; //reset the lastButtonPushed variable
}

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Well you can convert some parts of your code to actual C rather than "Wiring", this will also massively shrink you code

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Well you can convert some parts of your code to actual C rather than "Wiring", this will also massively shrink you code