Arduino Forum Arduino Due and AD725 How-to?
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
  • State Suggested Answer
  • Replies 16 replies
  • Answers 1 answer
  • Subscribers 392 subscribers
  • Views 1473 views
  • Users 0 members are here
  • ad725
  • due
  • arduino
Related

Arduino Due and AD725 How-to?

kizin
kizin over 11 years ago

Is there a good resource for getting started with the AD725 (or AD724) and the Arduino or Aduino Due? I need to make a gui (possibly using bitmaps) that outputs s-video and composite.

 

Thanks in advance

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    are you planning on trying to output / generate the composite color or RGB. RGB of course would be way easier than comp.

     

    Using timers directly to output pins to generate the basic sync HS and VS may also help with a stable display. I also think the ARM has DMA capability, the TI ARM (TIVA C) boards do so this also can off load the CPU from dealing with most of the output work

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kizin
    0 kizin over 11 years ago in reply to Robert Peter Oakes

    Thanks, Peter.

     

    The Due does have a DMA controller.

    Yes, RGB and the sync signals. How-to?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kizin
    0 kizin over 11 years ago in reply to Robert Peter Oakes

    Thanks, Peter.

     

    The Due does have a DMA controller.

    Yes, RGB and the sync signals. How-to?