Arduino
  • Products
  • More
Arduino
Arduino Forum How to power up intel galileo with a battery
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 417 subscribers
  • Views 844 views
  • Users 0 members are here
Related

How to power up intel galileo with a battery

e14 Contributor
e14 Contributor over 12 years ago

Sir i am using the intel galileo board which supports arduino 1.5.3 IDE. But in my project i want my robot moving with galileo on it.So how can i power up my galileo with a battery pack of 12v and the down convert it 5v and use it for galileo...plz help me

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    Use a low cost DC-DC converter, this would be the most efficient and therefore give you best battery consumption

     

    like one of these  NMXS1205UC MURATA POWER SOLUTIONS DC / DC Converters - Isolated Board Mount Single Output | 70K3967 | Newark element14 C…

     

    this is a quality one from Newark, you can also get ones from Ebay for a few $$ if your willing to wait http://www.ebay.com/sch/i.html?_from=R40&_trksid=p2047675.m570.l1313.TR3.TRC2.A0.H0.Xbuck+convertor&_nkw=buck+convertor&_sacat=0

     

    I am assuming you need at least 1A at 5V

     

    Hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    So can i use a linear regulated supply ...like 7805 with output current max 1.5A at 5V...? ...for powering the galileo...?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    element14jamie  ... Jamie, another thing to look at image

     

    Sorry you did not get a reply earlier, I responded directly from the email as it says I can but it is not showing up here, did you get a response ?

     

    anyway, Yes you could use a 7805 regulator but it would be very inefficient, much less than 50% as you would be dropping all 7V across it and at one amp thats 7W, add this to the 5W (Assuming 1A again) thats 12 W consumed for only 5W used

     

    A Buck converter will be in excess of 90% efficient as it is an energy converter, not a voltage dropper.

     

    Both will work, 7805 is cheaper but at the cost of heat and wasted power from the batteries

     

    Regards

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    element14jamie  ... Jamie, another thing to look at image

     

    Sorry you did not get a reply earlier, I responded directly from the email as it says I can but it is not showing up here, did you get a response ?

     

    anyway, Yes you could use a 7805 regulator but it would be very inefficient, much less than 50% as you would be dropping all 7V across it and at one amp thats 7W, add this to the 5W (Assuming 1A again) thats 12 W consumed for only 5W used

     

    A Buck converter will be in excess of 90% efficient as it is an energy converter, not a voltage dropper.

     

    Both will work, 7805 is cheaper but at the cost of heat and wasted power from the batteries

     

    Regards

     

    Peter