Arduino Forum OK, HELP!!! NRF24L01 Issues
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 392 subscribers
  • Views 315 views
  • Users 0 members are here
  • wireless
  • nrf24l01
  • communication
Related

OK, HELP!!! NRF24L01 Issues

funinalaska
funinalaska over 11 years ago

Ok,

I am having issues getting wireless communications to work on my Arduinos.

I have both the 433mhz simple modules that are one way only

and I have the NRF24L01 transceiver modules.

I tried yesterday with the 433mhz ones and I was getting things but things seemed scrambled and inconsistent which I have heard can be a problem with those.

So I decided to try today that NRF modules.

I hooked up 2 of them each to an UNO and am tryig the pingpong example sketch in the RF24 library.

I am getting nothing but "failed"

I have it hooked up to pins 2, 9, 10, 11, 12, 3.3v and GND

as is instructed in any tutorial I have seen on the example sketch.

I am getting very frustrated with these modules at this point.

So for now I am going to put it away and walk away for a bit.

Any words of advise or wisdom on the subject is greatly appreciated.

Thank you in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Former Member +1
    I used the NRF24L01 with my IoT of Holiday lights project, all the code is included in the various posts, this includes having multiple remote nodes talking to a single hub node, all various arduino boards…
Parents
  • Former Member
    0 Former Member over 10 years ago

    I'm having the same problems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to Former Member

    I used the NRF24L01 with my IoT of Holiday lights project, all the code is included in the various posts, this includes having multiple remote nodes talking to a single hub node, all various arduino boards

     

    BYOB Party #1, "Bring you own Bulbs" - The Internet of Holiday Lights

     

    Hope it helps

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Robert Peter Oakes

    Have you noticed that problems are easier to replicate than are solutions?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to Robert Peter Oakes

    Have you noticed that problems are easier to replicate than are solutions?

    Clem