Arduino
  • Products
  • More
Arduino
Arduino Forum servo motor for micro arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 419 subscribers
  • Views 1049 views
  • Users 0 members are here
  • arduino
Related

servo motor for micro arduino

e14 Contributor
e14 Contributor over 11 years ago

guys is servo motor compatible with arduino micro ?

i couldn't find an answer anywhere for specifically arduino micro

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Most servo motors that are the kind found in model planes and cars are easy to interface with an Arduino and there are libraries to make life easy to to code it. If you are looking at a servo motor other than this, you may have to include a motor control board, also been done hundreds of times before

     

    provide more details f=of the parts you intending to use and we can help in more detail

     

    Regards


    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    thanks for replying peter

    image

    so this is an ipad case that im making and the ipad would be placed in side,

    what im going to do is that i want the case to slide open automatically with a keyboard command through a button connected to arduino.

    im thinking of using servo motor and crank slide mechanism to slide it open..but i was not sure that arduino micro would support this..i dont think the weight would be so much so i guess a regular servo motor would be able to handle this.

    so any suggestion would be really appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • timswift
    0 timswift over 11 years ago in reply to e14 Contributor

    The arduino micro can control up to 7 RC servos.

     

     

     

     

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nschreiber0813
    0 nschreiber0813 over 11 years ago in reply to timswift

    Dear: Tim

    Yes it can handle servos but I would recommend using a servo shield for what you are doing. It is way more practical than arduino micro and if have problems with it I recommend you build your own. Also here is some code for you.

    From: Noah

     

    // Sweep

    // by BARRAGAN <http://barraganstudio.com>

    // This example code is in the public domain.

     

     

     

     

    #include <Servo.h>

     

    Servo myservo;  // create servo object to control a servo

                    // a maximum of eight servo objects can be created

     

    int pos = 0;    // variable to store the servo position

     

    void setup()

    {

      myservo.attach(9);  // attaches the servo on pin 9 to the servo object

    }

     

     

    void loop()

    {

      for(pos = 0; pos < 180; pos += 1)  // goes from 0 degrees to 180 degrees

      {                                  // in steps of 1 degree

        myservo.write(pos);              // tell servo to go to position in variable 'pos'

        delay(15);                       // waits 15ms for the servo to reach the position

      }

      for(pos = 180; pos>=1; pos-=1)     // goes from 180 degrees to 0 degrees

      {                               

        myservo.write(pos);              // tell servo to go to position in variable 'pos'

        delay(15);                       // waits 15ms for the servo to reach the position

      }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • nschreiber0813
    0 nschreiber0813 over 11 years ago in reply to timswift

    Dear: Tim

    Yes it can handle servos but I would recommend using a servo shield for what you are doing. It is way more practical than arduino micro and if have problems with it I recommend you build your own. Also here is some code for you.

    From: Noah

     

    // Sweep

    // by BARRAGAN <http://barraganstudio.com>

    // This example code is in the public domain.

     

     

     

     

    #include <Servo.h>

     

    Servo myservo;  // create servo object to control a servo

                    // a maximum of eight servo objects can be created

     

    int pos = 0;    // variable to store the servo position

     

    void setup()

    {

      myservo.attach(9);  // attaches the servo on pin 9 to the servo object

    }

     

     

    void loop()

    {

      for(pos = 0; pos < 180; pos += 1)  // goes from 0 degrees to 180 degrees

      {                                  // in steps of 1 degree

        myservo.write(pos);              // tell servo to go to position in variable 'pos'

        delay(15);                       // waits 15ms for the servo to reach the position

      }

      for(pos = 180; pos>=1; pos-=1)     // goes from 180 degrees to 0 degrees

      {                               

        myservo.write(pos);              // tell servo to go to position in variable 'pos'

        delay(15);                       // waits 15ms for the servo to reach the position

      }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to nschreiber0813

    well the reason i wanna use micro is i want to have a serial communication with the keyboard..so basically control the movement by keyboard and eventually a remote control..

    so do you think it will be ok using one servo motor with micro!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    The only real advantages of the Shield is increased number of PWM outputs and an increase in resolution from 8Bits to 12Bits which is the same as 0-255Count vs 0-4096 count. If you don't need better than a 1.4 - 2 degree resolution then the direct Arduino will work just fine, if you need real precision then go for the shield, but based on your description, I don't think you will need it. The other thing to bear in mind, you may be able to power one servo from the Arduino supply but not more, the preference is to provide a separate 5V for the servos.

     

    Regards

     

     

    Peter