Arduino
  • Products
  • More
Arduino
Arduino Forum Overflowing numbers
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 415 subscribers
  • Views 653 views
  • Users 0 members are here
  • structures
  • rtc
  • c++
  • data
Related

Overflowing numbers

Workshopshed
Workshopshed over 11 years ago

I was working with a DS3107 Real Time Clock module and the Time library. I've been using the tmElements_t structure to pass the data. This is defined as follows:

 

typedef struct  { 
  uint8_t Second; 
  uint8_t Minute; 
  uint8_t Hour; 
  uint8_t Wday;   // day of week, sunday is day 1
  uint8_t Day;
  uint8_t Month; 
  uint8_t Year;   // offset from 1970; 
} tmElements_t, TimeElements, *tmElementsPtr_t;

 

Each of the elements are defined as 8bit unsigned integers which is fine for the hours and minutes etc but when you come to the years there's a problem waiting to snare you.

 

tmElements_t tm;
tm.Year = 2014;

 

This code nicely compiles but will cause you a problem when it runs as 2014 will overflow the 8 bits available. It took me a few hours of experimenting and delving into the library to work out what was going on.

 

Is there a way I can trap for this overflow at compile time?

If not is there an alternative way of coding the time elements in C or C++ that can trap this?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 11 years ago

    Hi Andy,

     

    It's an interesting question. The coding as it stands should have generated a warning. Normally you would get a warning with a compiler, but possibly the IDE (is this Arduino?) may have suppressed it (I'm not too familiar with the Arduino IDE unfortunately - maybe there is an option in a menu). With gcc I see this:

    warning: large integer implicitly truncated to unsigned type [-Woverflow]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 11 years ago

    Hi Andy,

     

    It's an interesting question. The coding as it stands should have generated a warning. Normally you would get a warning with a compiler, but possibly the IDE (is this Arduino?) may have suppressed it (I'm not too familiar with the Arduino IDE unfortunately - maybe there is an option in a menu). With gcc I see this:

    warning: large integer implicitly truncated to unsigned type [-Woverflow]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Workshopshed
    0 Workshopshed over 11 years ago in reply to shabaz

    t seems that the Arduino IDE output from the compiler is either errors only or verbose. A lot of the core libraries seem to report warnings so it might be hard to spot this warning.

    Maybe for my next project I'll look at an alternative IDE and possibly swap Arduino platform for the AVR tools.