Arduino
  • Products
  • More
Arduino
Arduino Forum Assistance with Arduino Inputs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 419 subscribers
  • Views 909 views
  • Users 0 members are here
Related

Assistance with Arduino Inputs

e14 Contributor
e14 Contributor over 11 years ago

Hi, first time on the forums.  Sorry if this has been answered already, but my search-fu isn't returning anything helpful.

 

Here's my project:  I make busy lights.

 

I have my arduino all coded and happy so that when a momentary switch is pressed (built in pull-up resistor), a relay is turned on and a series of LED lights make a very pretty lighting animation until the momentary switch is let go and the entire board goes silent.  It's perfect.

 

Now comes the challenge.  I want the arduino to be "triggered" by an external event.

 

I've taken apart my wireless headset, desoldered one of the LEDs and extended those leads to my breadboard.  So now, when I pick up my phone with the headset, I've got an LED that lights up on my breadboard.  Nice!

 

Now my question, how to connect the two?  I want the LED light from the headset to trigger the arduino just like the momentary switch does now.

 

I've tried using digitalRead on Pin9 (doesn't change the value, shows "0")

I've tried using analogRead on Pin9(doesn't change the value reported to the Arduino)

 

I feel like I'm missing something simple, a way for the arduino to detect voltage from an outside source (the LED reports either zero voltage (headset is not on) or 2 volts (headset is on, LED is lit up).

 

If this isn't enough information, I can prototype everything on Fritzing and post the file, or I can post my arduino code, but I have a feeling someone is going to say, "use the BLAH" and maybe point me to a link that I can take and run with.

 

Sorry for the wall of text, appreciate those who read till the end.

 

Thanks,

 

Aaron

  • Sign in to reply
  • Cancel

Top Replies

  • bobcroft
    bobcroft over 11 years ago +1 verified
    Aaron, Have you correctly configured your Arduino I/O as inputs? Have you tried setting the internal pull up on the input pin? the output to the LED on the headset may be open collector. That would need…
  • e14 Contributor
    e14 Contributor over 11 years ago +1
    You guys are amazing! Thanks for the responses. The problem was two-fold (wrong input pin and too low voltage for Arduino to recognize). I didn't know to use A0 (analog zero) as the input and was using…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    With a 5V uController, 2V may not quite be enough to allow the Arduino to read a one, using one of the alalogue inputs should have read something though, you have got a common ground right ?, connecting the low side (Volts wise) of the LED to the GND of the Arduino

     

     

     

    Another option is to power a transistor base, say a 2n2222 or similar to drive the input to ground and also allow it to go to the full voltage of the pullup inside the micro

     

     

     

    Regards

     

     

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    With a 5V uController, 2V may not quite be enough to allow the Arduino to read a one, using one of the alalogue inputs should have read something though, you have got a common ground right ?, connecting the low side (Volts wise) of the LED to the GND of the Arduino

     

     

     

    Another option is to power a transistor base, say a 2n2222 or similar to drive the input to ground and also allow it to go to the full voltage of the pullup inside the micro

     

     

     

    Regards

     

     

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer