Arduino
  • Products
  • More
Arduino
Arduino Forum servomotor (arduino)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 23 replies
  • Subscribers 418 subscribers
  • Views 3132 views
  • Users 0 members are here
  • ultrasonic_sensor
  • servo
  • arduino
Related

servomotor (arduino)

e14 Contributor
e14 Contributor over 11 years ago

Hello, I am looking for a program to monitor 4 servomotors by a detector ultrasonic HC-SR04 (external power supply). The movement of each servo is different.
I am totally beginner.

Thank you to all

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    You only mention one sensor but you have it monitoring for someone within 50cm and also monitoring the servos, are you using 2 sensors ?

     

    or is the sensor monitoring for people close to it, If detected it starts the servos (4 with their own actions), but if the person / object moves out of range of the sensor the servos will stop what ever there doing and wait for a new presence to be detected by the sensor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    the ultrasonic sensor (and servos) are attached to the wall. when a person approaches 50 cm or less, servos start in march.

    Yes, the sensor is monitoring for people close to it, If detected it starts the servos (4 with their own actions), but if the person moves out of range of the sensor the servos will stop what ever there doing and wait for a new presence to be detected by the sensor.

     

    Le 6 oct. 2014 à 20:54, peteroakes <messages@element14.com> a écrit :

     

    You only mention one sensor but you have it monitoring for someone within 50cm and also monitoring the servos, are you using 2 sensors ?

     

    or is the sensor monitoring for people close to it, If detected it starts the servos (4 with their own actions), but if the person / object moves out of range of the sensor the servos will stop what ever there doing and wait for a new presence to be detected by the sensor

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kidiccurus

    Wonderful !

    For the other two servo I place on pin 7 and 8 or 11 and 12 ?

    For supply of servos I plug how?

     

    Again thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    I Would suggest you use a separate 5v for the servo power, the arduino regulator will not be happy driving 4 servos

     

    Connect the servo +v pins to the power supply

    connect the ground (0v) of the servo supply to the gnd pin on the arduino,

    connect the 0v of the servo supply to all the servos

    the pwm pins are connected as indicated above

     

    THat at should get you running nice and reliably

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to e14 Contributor

    Oh, sorry, I made a mistake, I thought you only had 2 servos. Please just tell me how many of each type of servo you have so I can alter the progran accordingly. I agree that you should be using an external PSU for that many servos. Also, a quick request, when we get this working could you please post a video, I really want to see this cool piece of art that you have made.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Thank You.

    I have either a battery of 4 x 1.5 V or an AC / DC power adapter, model TSL-0901, output 9V DC 1000mA.
    Which is best ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kidiccurus

    For now I have 2 Tower Pro servos and 2 Futaba servos (Do you know larger models at a reasonable price?).
    For now I'm trying to solve the practical and technical problem. I attack the artistic part in January. Once the installation is finished I will post a photo or video (how?).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to e14 Contributor


    #define echoPin 12 
    #define trigPin 13 
    #include <Servo.h>  
    Servo towerpro; 
    Servo futaba;
    Servo towerpro2; 
    Servo futaba2; 
    void setup() { 
      Serial.begin (9600); 
      pinMode(trigPin, OUTPUT); 
      pinMode(echoPin, INPUT); 
       
      towerpro.attach(9); 
      futaba.attach(11);
      towerpro2.attach(10); 
      futaba2.attach(12);  
      towerpro.write(90); 
      futaba.write(30);
      towerpro2.write(90); 
      futaba2.write(30);  
      randomSeed(analogRead(0)); 
    } 
     
    void loop() { 
    start: 
      long duration, distance; 
      digitalWrite(trigPin, LOW);  // Added this line 
      delayMicroseconds(2); // Added this line 
      digitalWrite(trigPin, HIGH); 
    //  delayMicroseconds(1000); - Removed this line 
      delayMicroseconds(10); // Added this line 
      digitalWrite(trigPin, LOW); 
      duration = pulseIn(echoPin, HIGH); 
      distance = (duration/2) / 29.1; 
      if (distance < 20) {  // Change value 20 to change trigger distance 
        goto start; 
    } 
     
      if (distance >= 200 || distance <= 0){ 
        Serial.println("Out of range"); 
      } 
      else { 
        Serial.print(distance); 
        Serial.println(" cm"); 
      } 
      delay(100); 
      towerpro.write(random(0,180)); 
      futaba.write(random(0,60));
      towerpro2.write(random(0,180)); 
      futaba2.write(random(0,60));  
      delay(random(250,2000)); 
    } 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to kidiccurus

    Ok, all your servos should now work. The tower pro servos go to pins 9 and 10 and the futaba servos to pins 11 and 12. As for power, I recommend a high power usb charger or even a pc psu. If you cut open a usb cable then the red wire is power and the black wire ground. Make sure you do not use tis on a pc as it will require too much power and may damage your usb ports. For testing purposes you might be able to use the Arduino to supply power if you only hook up 1 servo at a time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kidiccurus

    message d'Arduino :

    sketch_oct23a:49: error: redefinition of 'Servo towerpro'

    sketch_oct23a:4: error: 'Servo towerpro' previously declared here

    sketch_oct23a:50: error: redefinition of 'Servo futaba'

    sketch_oct23a:5: error: 'Servo futaba' previously declared here

    sketch_oct23a.ino: In function 'void setup()':

    sketch_oct23a:53: error: redefinition of 'void setup()'

    sketch_oct23a:6: error: 'void setup()' previously defined here

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    9V will be too high for the servos probably so unless you have a DC-DC converter or a 5V regulator it may be better to go with the 4*1.5V batteries

     

     

     

    Regards

     

     

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    I think the code was accidentally pasted twice, delete the second copy of the declarations, Setup() and Loop() methods etc then it should work

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    I think the code was accidentally pasted twice, delete the second copy of the declarations, Setup() and Loop() methods etc then it should work