Hi all
i have quite a few car relays and was wondering if i can use these in some projects
problem is i have been told that they need 12 volts to turn on
these relays say 12volts and 30Amps
i tried using one in a project a while ago and it didn't work the Arduino voltage wasn't enough
when i tried to power the relay with a 9v battery i heard it click
so i was thinking about stepping up the voltage to power the relay but dont know how to do this
i have seen boost converters on eBay but there about $15 and don't want to spent that much each and every
time i do a new project.
thing is i can get car relays for free and if i can use them without spending lots of money it would be good
i do realize that i can get relays pretty cheap but if i can use the ones i have with out too much difficulty
and spending lots of money i will be happy.
these are 4 pin relays 12V , 30A