Arduino
  • Products
  • More
Arduino
Arduino Forum Need coding help.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 425 subscribers
  • Views 1476 views
  • Users 0 members are here
  • arduino
Related

Need coding help.

e14 Contributor
e14 Contributor over 11 years ago

So I have never coded anything before in my life and I found this community from the jeremy blum youtube videos.

 

I am building a vivarium (snake cage) and would like to fully automate the temperature and humidity for it and be able to monitor and adjust the temp and humidity wirelessly over my home network. I have done a lot of research on my own and think I have all of the right parts I just need help with the coding and one small wiring connection. I will list as many details as possible below and I would love if someone here would be able to help and teach me!

 

PARTS LIST: Arduino uno r3, AM2302 (wired DHT22) temperature-humidity sensor, adafruit cc3000 WiFi shield with onboard ceramic antenna, Sain smart 4 channel solid state relay (load: 2A, 240VAC, 50/60Hz), Humidifier runs on 30 watts 120V, Ceramic heat lamp 100 watts, shield stacking headers for arduino r3, breadboard, wires, and resistors.

 

What I would like is the sensor to be in the cage (hence the AM2302 not just the DHT22) and the rest of the components outside. I would have the parameters set (Ex: 83 *F and 85% RH) and any time the actual temperature or humidity fell below those values the ceramic heat lamp and/or humidifier would turn on until those values have been reached and then they would turn off. Finally (and not a fully necessary requirement) have the data wirelessly sent to my computer over my home network so I can see actual temperature and humidity at that time and change it if so desired and a graph of temperature/humidity over time. This part is not needed I just would like it if it is possible to do.

 

As stated I have no experience in coding but I am handy with electronics and quick to learn. I do not know how difficult something like this is I just know it is way over my head.

 

If there is any information missing or any questions feel free to ask!!

 

Thank you in advance!

  • Sign in to reply
  • Cancel

Top Replies

  • fvan
    fvan over 11 years ago +2
    Hi, that's a challenging project you're taking on Perhaps it would be good to experiment with more basic things first, like the temperature sensor only, and gradually build coding knowledge. The Arduino…
  • markvenn
    markvenn over 11 years ago +2
    Hi I have to agree with Frederick on this, start small and build on this small start. As you work through one bit at a time you will very quickly build up your knowledge and you will find that you won…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    This may help, a video I produced a while ago DHT22 temperature and Humidity Sensor with Arduino Uno and Ethernet Card (ENC or WizNet) (Instant weather Station) also Driving BIG loads with your micro controller…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    I hate to be 'that guy,' but:  If your snakes are waiting on this, my friend has snakes, they are quite sensitive to environmental params, you could get a pair of temperature controllers to manage your humidity and temperature and work on the uP solution at your leisure.  I got a controller for a hunny from ebay and a big SSR and put them into a cabinet.  I put a linear humidity probe at the end of a cable with a stereo jack.  I got the controller to interpret the sensor signum and scale as a temp sensor running form 0 to 100 C.   In a coupla hours I had my humidifier under PID control with DRO!

     

    POTS to the rescue!  IIRC it's a Canon XLR connector I have the humidity probe on.  I was able to take one apart and solder the sensor to a terminus so that I can use POTS XLR extension cords if need be.  Sure is fun to watch the numbers bobble!  SP is displayed as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    I hate to be 'that guy,' but:  If your snakes are waiting on this, my friend has snakes, they are quite sensitive to environmental params, you could get a pair of temperature controllers to manage your humidity and temperature and work on the uP solution at your leisure.  I got a controller for a hunny from ebay and a big SSR and put them into a cabinet.  I put a linear humidity probe at the end of a cable with a stereo jack.  I got the controller to interpret the sensor signum and scale as a temp sensor running form 0 to 100 C.   In a coupla hours I had my humidifier under PID control with DRO!

     

    POTS to the rescue!  IIRC it's a Canon XLR connector I have the humidity probe on.  I was able to take one apart and solder the sensor to a terminus so that I can use POTS XLR extension cords if need be.  Sure is fun to watch the numbers bobble!  SP is displayed as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • markvenn
    0 markvenn over 11 years ago in reply to D_Hersey

    Very good points here. If you are going to set up a system like this I suppose you should do a dry run to make sure all the bits work properly, dont want your scaly friends overheating. I know they are cold blooded and need warming but we don't want to overdo it. Let us know hoe you get on!