Arduino Forum Multiple Arduino functions without delay
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
  • State Not Answered
  • Replies 20 replies
  • Subscribers 395 subscribers
  • Views 2566 views
  • Users 0 members are here
  • timers
  • arduinouno
  • delay
  • interval_timer
  • delay_interval
  • led
  • arduino
  • solenoid
Related

Multiple Arduino functions without delay

Former Member
Former Member over 10 years ago

I have literally zero coding experience but have run into the need for it at my job -- all help appreciated. Basically, I am trying to accomplish many things at once and am not sure how to translate what i need into code. What I need: a tone and a light to simultaneously flash on for 500 milliseconds and then off again for 6 seconds; water reward to be delivered (by turning on/ off a solenoid) 2 seconds after the tone/LED have turned off, with the solenoid being open for 25 milliseconds; continuous collection of data from an input potentiometer. Since i need to monitor the input from the potentiometer at all times, i cannot use "delay()" because i cannot have the board stop reading the values from the potentiometer to preform a function.

 

This is a code i attempted -- however, the issue is the timing for the LED/tone and the solenoid. I need the solenoid to always open 2 seconds after the LED/tone turn off and it needs to open for 25 milliseconds and then shut back off. i have put hours into trying to figure out a way to do this --- as the code is now, the led/tone turn on and off fine, but the solenoid has a longer delay time (because i was trying to get it to come 2 seconds after the led/tone went off) and the excess time builds onto itself and makes the timing of the solenoid vary in its proximity to the LED/tone.

 

#include <elapsedMillis.h> //the timer.

 

 

//stopwatches

elapsedMillis timer; 

 

 

int ledPin = 11;

int lick = 4;

int solenoid = 8;

int speaker = 2;

int ledOn = 500;       //milliseconds

int ledOff = 6000;

int solenoidOn = 25;

int solenoidOff = 8475;

int LickState;

 

 

int playTime = 500;  //how long speakers will play for

int freq = 8000;  //frequency for left prize speakers in hz

int toneTime = 500;

 

 

unsigned long lms;        //time from millis()

unsigned long lmsLast;    //last time the LED changed state

unsigned long sms;        //time from millis()

unsigned long smsLast;

unsigned int LedOn = 0;

unsigned int Reward = 0;

unsigned int Lick = 0;

boolean ledState;        //current LED state

boolean solenoidState;

 

 

void setup(void){

  Serial.begin(9600);

  pinMode(lick, INPUT); 

  pinMode(ledPin, OUTPUT);

  pinMode(solenoid, OUTPUT);

  pinMode(speaker, OUTPUT);

 

 

  elapsedMillis timer = 0;

}

 

 

void loop(void){

  int ledState = digitalRead(ledPin);

  int lickstate = digitalRead(lick);

  if (lickstate == HIGH){

//    Serial.println(lickstate);

    Serial.println(timer); }

  lms = millis();

    blinkLED();

  sms = millis();

    blinkLED();

   

 

} }

 

 

void blinkLED(void){

 

 

    if (lms - lmsLast > (ledState ? ledOn : ledOff)) {

        digitalWrite(ledPin, ledState = !ledState);

        lmsLast = lms;

        tone (speaker, freq, toneTime);

        Serial.print("Led");

        Serial.println(timer);

    }

    if (sms - smsLast > (solenoidState ? solenoidOn : solenoidOff)) {

        digitalWrite(solenoid, solenoidState = !solenoidState);

        smsLast = sms;

        Serial.print("Reward");

        Serial.println(timer);

    }

}

 

I have tried using if then statements to say that if the LED state is HIGH, then wait 2 seconds and deliver the reward --- the issue is the "wait 2 seconds part". how do i get the arduino to add two seconds to the current time when the LED turns off and then give my 25 millisecond reward without messing up the on/off times of the LED? Very confused.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +1
    This is a classic problem when creating real-time systems (which this is, since you want things to occur at or within certain times). Writing code without an OS to provide real time capabilities is difficult…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    here is an alternate approach you can try

     

    I have not included the actual digital IO, you already know how to do that but it does use a rudimentary state machine that should work for you and is easy extended if you need

     

    the code does compile on an arduino but I have not uploaded or tested it yet

     

    it will run every 6 seconds, will never re-run until the state machine is complete and reached the 6 seconds (Or should behave that way image )

     

    hope it helps, I will try to execute it and verify i got it right over the next few days but you can have a look now and try it for your self if you feel lucky image

    // constants
    #define  solenoidOnTime 25 // 25mS
    #define  LEDBuzzerTime 500 // 500mS
    #define  SolenoidDelayTime 2000 // 2 seconds
    #define  LoopTime 6000 // 6 seconds
    
    #define LEDPin 8
    #define BUZZERPin 9
    #define SOLENOIDPin 11
    
    //variables
    double LoopTrigger = 0; // loop timer
    int stateMachineValue = -1; // state tracker “-1” = waiting for trigger
    double nextState = 0; // used by the state machine function for timing
    
    void setup()
    {
      Serial.begin(9600); // add other initialization stuff
      LoopTrigger = millis();
      stateMachineValue = 0; // start state machine
    }
    
    void loop()
    {
      if ( (LoopTrigger <= (millis() - LoopTime)) && (stateMachineValue == -1)) // waiting for trigger and looptime has elapsed
      {
        stateMachineValue = 0 ; // start the state machine
        LoopTrigger = millis(); // reset loop timer, not this will not trigger until the state machine has completed
      }
      stateMachine();
    }
    
    void stateMachine()
    {
      switch (stateMachineValue)
      {
      case 0: 
        {
          nextState = millis();
          LEDBUZZERON();
          stateMachineValue ++; // next state
          break;
        }
      case 1: 
        {
          if(nextState <= (millis()-LEDBuzzerTime))
          {
            nextState = millis();
            LEDBUZZEROFF();
            stateMachineValue++; // next state
            break;
          }
        }
      case 2: 
        {
          if(nextState <= (millis()-SolenoidDelayTime))
          {
            nextState = millis(); 
            SOLENOIDON();
            stateMachineValue++; 
            break;
          }
        }
      case 3: 
        {
          if(nextState <= (millis()-solenoidOnTime))
          {
            nextState = millis(); 
            SOLENOIDOFF();
            stateMachineValue == -1;  // end state machine
            break;
          }
        }
        default:
        {
          LEDBUZZEROFF();
          SOLENOIDOFF();
        }
      }
    }
    void  LEDBUZZERON()
    {
      Serial.println("LED and Buzzer ON");
    }
    void  LEDBUZZEROFF()
    {
      Serial.println("LED and Buzzer OFF");
    }
    void  SOLENOIDON() 
    {
      Serial.println("LED and Buzzer ON");
    }
    void  SOLENOIDOFF() 
    {
      Serial.println("LED and Buzzer OFF");
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Robert Peter Oakes

    is this how it should all come together?

     

    #include <elapsedMillis.h> //the timer. 
    
    
    //stopwatches
    elapsedMillis timer;  
    
    
    // constants  
    int solenoidOnTime = 25; // 25mS  
    int LEDBuzzerTime  = 500; // 500mS  
    int SolenoidDelayTime = 2000; // 2 seconds  
    int LoopTime = 6000; // 6 seconds  
      
    int LEDPin = 8;
    int BUZZERPin = 9;  
    int SOLENOIDPin = 11;  
    int LICK = 4;
    
    
    int playTime = 500;  //how long speakers will play for
    int freq = 8000;  //frequency for left prize speakers in hz
    int toneTime = 500;   
      
      
    //variables  
    double LoopTrigger = 0; // loop timer  
    int stateMachineValue = -1; // state tracker “-1” = waiting for trigger  
    double nextState = 0; // used by the state machine function for timing  
      
    void setup()  
    {  
      Serial.begin(9600); // initialization stuff  
      pinMode(LICK, INPUT);  
      pinMode(LEDPin, OUTPUT); 
      pinMode(SPEAKERPin, OUTPUT);
      pinMode(SPOLENOIDPin, OUTPUT);
      LoopTrigger = millis();  
      stateMachineValue = 0; // start state machine  
      elapsedMillis timer = 0;
    }  
      
    void loop()  
    {  
      int lickstate = digitalRead(lick);
     if (lickstate == HIGH){
        //    Serial.println(lickstate);
        Serial.println(timer);  
        
      if ( (LoopTrigger <= (millis() - LoopTime)) && (stateMachineValue == -1)) // waiting for trigger and looptime has elapsed  
      {  
        stateMachineValue = 0 ; // start the state machine  
        LoopTrigger = millis(); // reset loop timer, not this will not trigger until the state machine has completed  
      }  
      stateMachine();  
    }  
      
    void stateMachine()  
    {  
      switch (stateMachineValue)  
      {  
      case 0:   
        {  
          nextState = millis();  
          LEDBUZZERON(); 
           
          stateMachineValue ++; // next state  
          break;  
        }  
      case 1:   
        {  
          if(nextState <= (millis()-LEDBuzzerTime))  
          {  
            nextState = millis();  
            LEDBUZZEROFF();  
            stateMachineValue++; // next state  
            break;  
          }  
        }  
      case 2:   
        {  
          if(nextState <= (millis()-SolenoidDelayTime))  
          {  
            nextState = millis();   
            SOLENOIDON();  
            stateMachineValue++;   
            break;  
          }  
        }  
      case 3:   
        {  
          if(nextState <= (millis()-solenoidOnTime))  
          {  
            nextState = millis();   
            SOLENOIDOFF();  
            stateMachineValue == -1;  // end state machine  
            break;  
          }  
        }  
        default:  
        {  
          LEDBUZZEROFF();  
          SOLENOIDOFF();  
        }  
      }  
    }  
    void  LEDBUZZERON()  
    {  
      Serial.println("LED and Buzzer ON");  
      Serial.println (timer)
    }  
    void  LEDBUZZEROFF()  
    {  
      Serial.println("LED and Buzzer OFF"); 
      Serial.println (timer) 
    }  
    void  SOLENOIDON()   
    {  
      Serial.println("Solenoid ON");  
      Serial.println (timer)
    }  
    void  SOLENOIDOFF()   
    {  
      Serial.println("Solenoid OFF");  
      Serial.println (timer)
    } 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to Former Member

    looks like your on the right track, keep it up

     

    I would be pleased to see your progress as you move forward

     

    If you need more help, please ask

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to Former Member

    looks like your on the right track, keep it up

     

    I would be pleased to see your progress as you move forward

     

    If you need more help, please ask

     

    Peter