Arduino
  • Products
  • More
Arduino
Arduino Forum Just got a Arduino Trinket
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 1609 views
  • Users 0 members are here
  • trinket
  • arduino
Related

Just got a Arduino Trinket

Anonymous-58970
Anonymous-58970 over 11 years ago

Hello i know i was  M.I.A here but im doing a Project biased on the Arduino Trinket Link Here ( it coming on 20 next week ) im going take my time on this build a 4 moisture sensor and a Pump control the Pump i took off from a Bug Spray 2 im link up for Extra Push Power and water 8 Big Wooden Pot 3 small Plastic one and the Arduino specs ATtiny85 on-board, 8K of flash, 512 byte of SRAM, 512 bytes of EEPROM so i need help on Basic Code To Compile can Any one help me in here ?

  • Sign in to reply
  • Cancel

Top Replies

  • Anonymous-58970
    Anonymous-58970 over 11 years ago in reply to timswift +1
    there off a Ant Killer Spray ran off by 4 AA Battery
  • Anonymous-58970
    Anonymous-58970 over 11 years ago in reply to timswift +1
    i have the L298HN IC chip and there L293D & L297 Will fit that Small Package the Solar Size the down side it use more PWM Pin i will read up more on the L293D and L297
  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Hi Pablo Garcia, What do you want to code ? I can help you in coding. You can L298HN / L293D motor driver too. If your motor draws more current than you can use two of these chips ( 2 x L298 ) in parallel…
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Pablo Garcia,

     

    What do you want to code ? I can help you in coding.

    You can L298HN / L293D motor driver too. If your motor draws more current than you can use two of these chips ( 2 x L298 ) in parallel connection. Thus it will not burn if it draws more current. As per the motor you have showed in above picture, only one L298 would be sufficient.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Anonymous-58970
    0 Anonymous-58970 over 11 years ago in reply to e14 Contributor

    I am limited on pins and i Found a Heli RC Transistor from ON Semi NTB 85N03G im looking for PDF Data Sheet  now i need a Water and Moisture Sensor up to 8 Wooden Pots i was Thinking if i can Raid a Sensor getting 7 bent copper Rod connect all 8 Wooden Pots then put the Sensor on pot 1 and 8 So it can Detect all 8 pots so the rod be near to each other so sensitivity wont be weaken also i was asking for some give a Link to a Schematic & code to a Sensor that will allow the Arduino check all 8 wooden pots

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Anonymous-58970
    0 Anonymous-58970 over 11 years ago in reply to Anonymous-58970

    I got a Power Supply for the Trinket got a 5 pack of those 0.9v to 5V 600MA im going to add another DC to DC a 3v to 5 to Power the 2 motors so far it look small to fit in that 2.5v Solar  and got a Case for the Pumps for that as well i dont know about that Transistor will be able to pull it weight might go for the RC Heli Transistor

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Anonymous-58970
    0 Anonymous-58970 over 11 years ago in reply to Anonymous-58970

    I got a Power Supply for the Trinket got a 5 pack of those 0.9v to 5V 600MA im going to add another DC to DC a 3v to 5 to Power the 2 motors so far it look small to fit in that 2.5v Solar  and got a Case for the Pumps for that as well i dont know about that Transistor will be able to pull it weight might go for the RC Heli Transistor

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Anonymous-58970
    0 Anonymous-58970 over 11 years ago in reply to Anonymous-58970

    This is the RC Heli oh yea tha Green PCB down there i killed 1 of 5 of the 0.9 to 5v trying to remove the USB i Killed the SMD 4R7 inductor the rest of it still good