Arduino
  • Products
  • More
Arduino
Arduino Forum need help with an arduino sketch
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 641 views
  • Users 0 members are here
Related

need help with an arduino sketch

e14 Contributor
e14 Contributor over 11 years ago

I need help with writing an arduino sketch, for an a-star 32u4 micro to accept input from an analogue joystick and convert the input to advanced packet serial to a robo claw 2x60a that is using encoders for position control of the motors to be like a servo.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to gadget.iom +1
    Supports all sorts of Interrupts, here is the CPU datasheet from Atmel http://www.atmel.com/images/7766s.pdf Same set as an ATMEGA328 used in the UNO so I would imaging you can also use them in the same…
Parents
  • Anonymous-237891
    0 Anonymous-237891 over 11 years ago

    What you have to do:

     

    -do an analog read on your joystick output wich should be from 0->5 V with 2.5 V as neutral

    -this mean in the code tha 0 is all the way to the left 512 in the middle and 1023 all the way to the right

    -then use the map() function to assign 0 -> 1023 to more meaningful numbers such as 0 -> 180 deg for servomotors for exemple.

    -then you can write a table which as the degrees as the index and the paket serial you have to send as a value.

     

    This way you can do for exemple:

    print(paketSerial[readDegree]);

    this will send the serial paket corresponding to your analog read.

     

    Hope this helps. Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Anonymous-237891
    0 Anonymous-237891 over 11 years ago

    What you have to do:

     

    -do an analog read on your joystick output wich should be from 0->5 V with 2.5 V as neutral

    -this mean in the code tha 0 is all the way to the left 512 in the middle and 1023 all the way to the right

    -then use the map() function to assign 0 -> 1023 to more meaningful numbers such as 0 -> 180 deg for servomotors for exemple.

    -then you can write a table which as the degrees as the index and the paket serial you have to send as a value.

     

    This way you can do for exemple:

    print(paketSerial[readDegree]);

    this will send the serial paket corresponding to your analog read.

     

    Hope this helps. Cheers