Arduino
  • Products
  • More
Arduino
Arduino Forum ULN2003A driving IRF540N mosfet
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 34 replies
  • Answers 1 answer
  • Subscribers 420 subscribers
  • Views 8831 views
  • Users 0 members are here
Related

ULN2003A driving IRF540N mosfet

wallarug
wallarug over 11 years ago

Hey guys,

 

I am trying to expand the number of outputs on a board that I built 6 months ago that controls high current LED strips but am unsure if the following would work. Could someone please let me know if what I am trying to do in the following schematic will even work??

 

Thanks is advance.

 

imageimage

 

PS: I am aware of the 'negative logic' on the march 2014 version.

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Like this image

     

    "Here's one I prepared earlier"

     

    http://www.element14.com/community/groups/internet-of-things/blog/2014/08/05/drive-big-things-with-added-safety-opto-isolators

     

    Regards

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to Robert Peter Oakes

    Trust you to have polished your crystal ball.  image

     

    I always cringe when expensive hardware is not protected ...

    The advantage of the opto-couplers is they can be remote from the processor, and even duplicated.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 11 years ago in reply to mcb1

    I have read through Peter's post linked above.

     

    Very wise indeed.  I think this is a good idea for this project.

     

    Can you suggest a particular model of OPTO Isolator ?  I will need 14 outputs in total, so the more on a single chip the better! image  I will probably buy them from Jaycar:  www.jaycar.com.au

     

    On a side note:  What program do you use to draw up all your schematics?  I have tried a few but none of them seem as good as the schematics that are produced on this site and others.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to wallarug

    I see he's using an unlicensed copy of Johnny Cad and added his own logo.....This is simply terrible! image

     

    Wasn't the optoisolator the preferred method last time this was raised BTW?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to Problemchild

    unlicensed copy of Johnny Cad

    Yes but his isn;t the Johnny version.

     

    Wallarug

    I can't recommend any particular one, but you could try the 4 pin versions.

    Jaycar only seem to have 6 pin single channel.

     

    Since you are down under you could always try element14.co.au

    This one is 16 pin 4 channel and most seems to have Ic = 50mA, and 300% transfer (ie 1mA LED gives 3mA Collector)

    http://au.element14.com/vishay/k844p/opto-coupler/dp/1328383

     

    Toshiba have some multi channel higher current but MUCH higher price.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 11 years ago in reply to Problemchild
    Wasn't the optoisolator the preferred method last time this was raised BTW?

     

    No.  This is the first time I have heard of a optoisolator.  In the last discussion no-one even suggested them, which is why I was a bit confused when they came up here.

     

    Link to previous discussion:  http://www.element14.com/community/message/113013/l/arduino-and-transistors-question--re-school-musical-production#11301…

     

    I will take a detailed look at everything that everyone has posted on this thread and consider what I might do.

     

    >> I see he's using an unlicensed copy of Johnny Cad and added his own logo.....This is simply terrible!

    I don't think any version of Johnny Cad is going to cut it for the project I have in mind.  Is there an more digital alternative to Johnny Cad?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to wallarug

    Actually the opto-coupler did come up in reply #105

    http://www.element14.com/community/message/114536/l/re-arduino-and-transistors-question--re-school-musical-production#114536

     

    To be fair optoisolator and optocoupler are basically the same device.

    Sometimes the 'isolator' can have a mechanical interrupter (ie mouse wheel, door switch, end stop) that breaks the link between the LED and detector.

     

    You have obviously gotten to the point where your skills are being used more and more.

    This is the opportunity to plan for the future and make the board/boards able to be multiversal.

     

    If you make the board with an optocoupler and bring out both the Anode and Cathode along with the ability to change the series resistance, then it could be driven by almost anything you want.

    Several could even be run in parallel, and at some distance from the controller, or switch bank or whatever.

     

    I did this once with a Jackpot system controller which switched 24vAC and was perfect when one establishement wanted two signs linked together.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 11 years ago in reply to wallarug

    Actually the opto-coupler did come up in reply #105

    http://www.element14.com/community/message/114536/l/re-arduino-and-transistors-question--re-school-musical-production#114536

     

    To be fair optoisolator and optocoupler are basically the same device.

    Sometimes the 'isolator' can have a mechanical interrupter (ie mouse wheel, door switch, end stop) that breaks the link between the LED and detector.

     

    You have obviously gotten to the point where your skills are being used more and more.

    This is the opportunity to plan for the future and make the board/boards able to be multiversal.

     

    If you make the board with an optocoupler and bring out both the Anode and Cathode along with the ability to change the series resistance, then it could be driven by almost anything you want.

    Several could even be run in parallel, and at some distance from the controller, or switch bank or whatever.

     

    I did this once with a Jackpot system controller which switched 24vAC and was perfect when one establishement wanted two signs linked together.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • wallarug
    0 wallarug over 11 years ago in reply to mcb1

    mcb1 wrote:

     

    Actually the opto-coupler did come up in reply #105

    http://www.element14.com/community/message/114536/l/re-arduino-and-transistors-question--re-school-musical-production#114536

     

    Aha!  So they did...

     

    Must have skipped over those responses at the time (10 days before the musical started - lighting order due in 3 days).

     

    Some of them are very interesting, and sort of complicated for what I want to do.

     

    What are the chances of the MOSFET breaking anyway?

     

    I was doing a bit of research last night on the different ways and reasons that MOSFETs fail.  I found this website particularly interesting:  4QD Information Section

     

    In summary:

    • Too much voltage supplied (either to the gate or source/drain) 12 VDC is well inside the allowable limits of IRF540 (which is max 100V)
    • Too much current supplied (source/drain) only going to be supplying 0.5A on average maybe up to 1.0A at times through MOSFET (way inside max allowed: 33A)
    • dV/dt failure Not controlling motors, so I should be right on this one.
    • Excess Power dissipation Like before, using the MOSFET way inside its limit
    • "Foreign Object Failure"
    • Short-Circuit

     

    Of the list above, only two of them could possibly cause a massive failure in the MOSFET:

    1. Foreign Objects (leading to...)
    2. Short Circuit

     

    If a short circuit did occur (which still has a low chance when one is being extremely careful), then having an opto-coupler between the controller and the board would be nice.  I was thinking of making a sort of 'complimentary' buffer board with opto-couplers on it.  Maybe I could just buy one to save on the soldering.


    I will have a poke around on Element14 AU and see what they have.


    Replies to messages that came while I was typing this one (reverse order):

     

    0. Noted.   Thanks peter.

    1. I will give eagle cad free a go.

    2. Thank you for all the links.  I will have a look once this is submitted.

    3. More knowledge / information on  opto-couplers --> thank you for informing me on differing terminology.