Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Sensor that can pick up insect activity
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 6 answers
  • Subscribers 420 subscribers
  • Views 5146 views
  • Users 0 members are here
  • insect
  • arduino
  • sensor
Related

Sensor that can pick up insect activity

johaboo
johaboo over 11 years ago

Hi Everyone,

 

This is my first post so I wasn't to sure where to put this, this looked like the best place.

 

Anyway, I have a project I want to do where I use an Arduino to detect insects, specifically whiteflies.

 

My problem is I'm not sure what type of sensor would be best suited for this application, since whiteflies are extremely small, I wanted to make use of a sonar setup to detect them when they swarm, but I am unsure if the resolution on a sonar module would be enough to detect them.  This will happen in a closed greenhouse area so I'm not concerned about picking up unknowns and things. 

 

I would like to be able to detect them at a range of about 100mm min and 500mm max, and they measure around 1-2mm each, at the bear minimum I would like to know that there are a couple flying around the location of the sensor,  I do not need to know how many, and I would be happy if the sensor would be able to pick up only if there is a reasonable number.

 

So if anyone has any suggestions please speak up.

 

Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +4 suggested
    Hi Josephus, I had some time tonight so I bead boarded a simple circuit using an LED, a phototransistor,and an OP Amp. I hooked an oscilloscope up to the output of the Op Amp so I could monitor any signal…
  • jw0752
    jw0752 over 11 years ago +1 suggested
    Hi Josephus, Chances are that these insects have a wing beat frequency. If you can determine what that frequency is and select for it, then perhaps you could hear them with a sensitive microphone at a…
  • D_Hersey
    D_Hersey over 11 years ago +1 suggested
    A bug zapper and a current sensor or microphone? [non-non-destructive testing]
Parents
  • dougw
    0 dougw over 11 years ago

    Most of the sensor technologies that might meet your requirements will require high end (expensive) sensors and significant research to make them work in this application. You might try a sensitive ultrasonic microphone, but this is a long shot. You could try a video camera, pointed at a backlight white background, but this will probably require more horsepower than an arduino for image recognition.

    You could try a matrix of low-power laser beams and corresponding sensors. The lasers would need very narrow beams which is not easy to achieve. A single laser beam could be reflected many times to create a grid with one laser, but this requires very high quality mirrors in a very stable frame.

    With decent optics, you could create a "line" laser with one laser - which is like a curtain and have a row of pinhole sensors to detect where/when the curtain is interrupted.

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago

    Most of the sensor technologies that might meet your requirements will require high end (expensive) sensors and significant research to make them work in this application. You might try a sensitive ultrasonic microphone, but this is a long shot. You could try a video camera, pointed at a backlight white background, but this will probably require more horsepower than an arduino for image recognition.

    You could try a matrix of low-power laser beams and corresponding sensors. The lasers would need very narrow beams which is not easy to achieve. A single laser beam could be reflected many times to create a grid with one laser, but this requires very high quality mirrors in a very stable frame.

    With decent optics, you could create a "line" laser with one laser - which is like a curtain and have a row of pinhole sensors to detect where/when the curtain is interrupted.

    Doug