Arduino Forum Sensor that can pick up insect activity
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
  • State Suggested Answer
  • Replies 16 replies
  • Answers 6 answers
  • Subscribers 406 subscribers
  • Views 4302 views
  • Users 0 members are here
  • insect
  • arduino
  • sensor
Related

Sensor that can pick up insect activity

johaboo
johaboo over 11 years ago

Hi Everyone,

 

This is my first post so I wasn't to sure where to put this, this looked like the best place.

 

Anyway, I have a project I want to do where I use an Arduino to detect insects, specifically whiteflies.

 

My problem is I'm not sure what type of sensor would be best suited for this application, since whiteflies are extremely small, I wanted to make use of a sonar setup to detect them when they swarm, but I am unsure if the resolution on a sonar module would be enough to detect them.  This will happen in a closed greenhouse area so I'm not concerned about picking up unknowns and things. 

 

I would like to be able to detect them at a range of about 100mm min and 500mm max, and they measure around 1-2mm each, at the bear minimum I would like to know that there are a couple flying around the location of the sensor,  I do not need to know how many, and I would be happy if the sensor would be able to pick up only if there is a reasonable number.

 

So if anyone has any suggestions please speak up.

 

Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +4 suggested
    Hi Josephus, I had some time tonight so I bead boarded a simple circuit using an LED, a phototransistor,and an OP Amp. I hooked an oscilloscope up to the output of the Op Amp so I could monitor any signal…
  • jw0752
    jw0752 over 11 years ago +1 suggested
    Hi Josephus, Chances are that these insects have a wing beat frequency. If you can determine what that frequency is and select for it, then perhaps you could hear them with a sensitive microphone at a…
  • D_Hersey
    D_Hersey over 11 years ago +1 suggested
    A bug zapper and a current sensor or microphone? [non-non-destructive testing]
Parents
  • Former Member
    0 Former Member over 9 years ago

    Hi ,

     

    I am interested in this solution. I want to go little bit further than detection, to terminate the mosquitoes.  There is a proof of concept from Intellectual Ventures (IV)

    Photonic Fence | Intellectual Ventures

    The IV has a patent,

     

    I also found this article from UC Riverside.Which might be of useful to you.

    https://spie.org/membership/spie-professional-magazine/spie-professional-archives-and-special-content/spie-professional-…

     

    Thanks

    Nattu

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to Former Member

    Nattu Dakshin

    Interesting, but I think the poster is gone long ago:

    LAST LOGGED IN

    December 11, 2014

    Sorry,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago in reply to Former Member

    Nattu Dakshin

    Interesting, but I think the poster is gone long ago:

    LAST LOGGED IN

    December 11, 2014

    Sorry,

    Clem