Arduino Forum Help on I2C question
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
  • State Not Answered
  • Replies 11 replies
  • Subscribers 394 subscribers
  • Views 861 views
  • Users 0 members are here
  • iot_holidaylights
  • sparkle_ball
Related

Help on I2C question

clem57
clem57 over 10 years ago

Looking for a method/device to address as I2C to turn on/off 12+ volts. It needs to be very small and can have an address set. I will have around 50 different addresses to control 3 lights.

 

Thanks

Clem

  • Sign in to reply
  • Cancel

Top Replies

  • bobcroft
    bobcroft over 10 years ago +1
    Clem, Not I2C but SPI. Have a look at Majenko.co.uk he does a 32 port IO expander board and up to 4 can be used on 4 wires from the Arduino i.e. 128 IO! I use these to drive banks of 8 relays via opto…
Parents
  • Workshopshed
    0 Workshopshed over 10 years ago

    How about one of the ATTiny range with a mosfet or transistor to drive the LED?

     

    Alternatively one of the bigger Atmel microcontrollers with something like an darlington buffer chip such as the ULM2003. That way each microcontroller could handle 7 outputs.

     

    @Shabaz has a point about loading the bus with 50 devices, you might need to do some current calculations to ensure the driver can handle that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Workshopshed
    0 Workshopshed over 10 years ago

    How about one of the ATTiny range with a mosfet or transistor to drive the LED?

     

    Alternatively one of the bigger Atmel microcontrollers with something like an darlington buffer chip such as the ULM2003. That way each microcontroller could handle 7 outputs.

     

    @Shabaz has a point about loading the bus with 50 devices, you might need to do some current calculations to ensure the driver can handle that?