Arduino Forum Experience with a humidity sensor?
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
  • State Suggested Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 403 subscribers
  • Views 1351 views
  • Users 0 members are here
  • sensors
  • humidity
Related

Experience with a humidity sensor?

Former Member
Former Member over 10 years ago

I'm working on an Arduino project logging humidity, temperature and air pressure in a sewer for 30 days at a time. The environment is very hostile, 99 - 100% humidity and full of sulphuric acid.  (The acid comes from hydrogen sulphide combining with the humidity).  The prototype works fine and I'm about to make the final version of the hardware for deployment into the sewer.

 

I'm using a HYT 221 humidity sensor and while it is supposed to be chemical resistant I have the funny feeling it is not going to last the desired month in the sewer.  I suspect that the housing I'm going to use (Jiffy box) will allow moisture in, even with an o-ring around the sensor.  I also need to have the air pressure sensor exposed and that has no filter or protection.

 

Has anyone else had any experience exposing sensors to hostile environments and not having them die?

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 10 years ago

    When I was in HS, they made humidity sensors by attaching a strain gauge to a curly-headed person's hair.

     

    Silicone RTV can be your friend.  SiO2 being pretty stable stuff.  I don't think a modern gauge has to be too sensitive to the environment you describe.  IIRC they are made of a porous membrane of chloro-fluronated polymer and gold electrodes to make it into a capacitor.

     

    Another way to measure humidity is to put a conductivity gauge on the cold side of a peltier cooler in order to determine dew point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 10 years ago

    When I was in HS, they made humidity sensors by attaching a strain gauge to a curly-headed person's hair.

     

    Silicone RTV can be your friend.  SiO2 being pretty stable stuff.  I don't think a modern gauge has to be too sensitive to the environment you describe.  IIRC they are made of a porous membrane of chloro-fluronated polymer and gold electrodes to make it into a capacitor.

     

    Another way to measure humidity is to put a conductivity gauge on the cold side of a peltier cooler in order to determine dew point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to D_Hersey

    Don,

     

    I was considering using lots of HOT GLUE in it's various chemical variants.  I think APE may be the winning chemical, but the glue sticks never say what they are made from image, so it could be trial and error!