Arduino Forum Experience with a humidity sensor?
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
  • State Suggested Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 403 subscribers
  • Views 1351 views
  • Users 0 members are here
  • sensors
  • humidity
Related

Experience with a humidity sensor?

Former Member
Former Member over 10 years ago

I'm working on an Arduino project logging humidity, temperature and air pressure in a sewer for 30 days at a time. The environment is very hostile, 99 - 100% humidity and full of sulphuric acid.  (The acid comes from hydrogen sulphide combining with the humidity).  The prototype works fine and I'm about to make the final version of the hardware for deployment into the sewer.

 

I'm using a HYT 221 humidity sensor and while it is supposed to be chemical resistant I have the funny feeling it is not going to last the desired month in the sewer.  I suspect that the housing I'm going to use (Jiffy box) will allow moisture in, even with an o-ring around the sensor.  I also need to have the air pressure sensor exposed and that has no filter or protection.

 

Has anyone else had any experience exposing sensors to hostile environments and not having them die?

  • Sign in to reply
  • Cancel
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    You may benefit from potting the components in epoxy wherever possible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to gadget.iom

    Do you have any pressure/temperature sensors in mind?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to gadget.iom

    "Do you have any pressure/temperature sensors in mind?"

     

    Not yet.  My prototype is using a 10 DOF (GY-87) only because I had it lying around.  I'll probably end up buying a dedicated pressure sensor.  For temperature I'm currently using thermistors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to gadget.iom

    "Do you have any pressure/temperature sensors in mind?"

     

    Not yet.  My prototype is using a 10 DOF (GY-87) only because I had it lying around.  I'll probably end up buying a dedicated pressure sensor.  For temperature I'm currently using thermistors.