Arduino
  • Products
  • More
Arduino
Arduino Forum GSM Shield not working. Any ideas?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Answers 2 answers
  • Subscribers 411 subscribers
  • Views 3002 views
  • Users 0 members are here
  • comms
  • fault_finding
  • arduino
  • micro_controller
  • gsm_shield
Related

GSM Shield not working. Any ideas?

markvenn
markvenn over 11 years ago

Hi

I am having trouble getting my new gsm shield to work on my mega adk. I am using the standard gsm library to use the demo gsm sketches and it is using the sim card that came with the shield.  I ma getting nothing out of  the serial monitor except the very first printouts saying that the system his running. For example if I upload the gsm scanner i get the message saying that the scanner is starting but I get nothing else output. I am using a power supply for the mega ( 9v) and the led that light up are the on and then the status one comes on and net flashes for a bit then all seems to go quiet.

 

Code as follows. I have added an extra function that is supposed to copy the imei of the modem but nothing happens except the output below appears.

/*

 

GSM Scan Networks

 

This example prints out the IMEI number of the modem,

then checks to see if it's connected to a carrier. If so,

it prints the phone number associated with the card.

Then it scans for nearby networks and prints out their signal strengths.

 

Circuit:

* GSM shield

* SIM card

 

Created 8 Mar 2012

by Tom Igoe, implemented by Javier Carazo

Modified 4 Feb 2013

by Scott Fitzgerald

 

http://arduino.cc/en/Tutorial/GSMToolsGsmScanNetworks

 

This example code is part of the public domain

*/

 

// libraries

#include <GSM.h>

 

// PIN Number

#define PINNUMBER ""

 

// initialize the library instance

GSM gsmAccess;     // include a 'true' parameter to enable debugging

GSMScanner scannerNetworks;

GSMModem modemTest;

 

// Save data variables

String IMEI = "";

 

// serial monitor result messages

String errortext = "ERROR";

 

void setup()

{

  // initialize serial communications and wait for port to open:

  Serial.begin(9600);

  while (!Serial) {

    ; // wait for serial port to connect. Needed for Leonardo only

  }

 

  Serial.println("GSM networks scanner");

  test();

  scannerNetworks.begin();

 

 

  // connection state

  boolean notConnected = true;

 

  // Start GSM shield

  // If your SIM has PIN, pass it as a parameter of begin() in quotes

  while(notConnected)

  {

    if(gsmAccess.begin(PINNUMBER)==GSM_READY)

      notConnected = false;

    else

    {

      Serial.println("Not connected");

      delay(1000);

    }

  }

 

  // get modem parameters

  // IMEI, modem unique identifier

  Serial.print("Modem IMEI: ");

  IMEI = modemTest.getIMEI();

  IMEI.replace("\n","");

  if(IMEI != NULL)

    Serial.println(IMEI);

}

 

void loop()

{

  // scan for existing networks, displays a list of networks

  Serial.println("Scanning available networks. May take some seconds.");

  Serial.println(scannerNetworks.readNetworks());

 

    // currently connected carrier

  Serial.print("Current carrier: ");

  Serial.println(scannerNetworks.getCurrentCarrier());

   

  // returns strength and ber

  // signal strength in 0-31 scale. 31 means power > 51dBm

  // BER is the Bit Error Rate. 0-7 scale. 99=not detectable

  Serial.print("Signal Strength: ");

  Serial.print(scannerNetworks.getSignalStrength());

  Serial.println(" [0-31]");

 

}

 

void test(){

    Serial.print("Modem IMEI: ");

  IMEI = modemTest.getIMEI();

  IMEI.replace("\n","");

  if(IMEI != NULL)

    Serial.println(IMEI);

}

 

OUTPUT:

=======

GSM networks scanner

Modem IMEI:

  • Sign in to reply
  • Cancel

Top Replies

  • markvenn
    markvenn over 11 years ago in reply to gadget.iom +1
    Hi Paul It is the GSM R3 telefonica shield on a mega adk r3 arduino
  • markvenn
    markvenn over 11 years ago in reply to gadget.iom +1
    I am just uploading the sketch now. I have checked the sim in a phone and it is happy to roam onto the o2 network here, telefonica own o2 so no surprise there. I am surprised by the power that can be drawn…
  • gadget.iom
    gadget.iom over 11 years ago in reply to markvenn +1 verified
    AHA! http://arduino.cc/en/Guide/GSMShieldLeonardoMega
Parents
  • hirayastudent
    0 hirayastudent over 9 years ago

    Good Day,

     

    I am using ATmega2560 and GSM shield 2 and I can send and receive SMS but the IMEI is 0. I attached a picture below. Pls help.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hirayastudent
    0 hirayastudent over 9 years ago

    Good Day,

     

    I am using ATmega2560 and GSM shield 2 and I can send and receive SMS but the IMEI is 0. I attached a picture below. Pls help.image