Arduino Forum Arduino - RFID/Keypad lock
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 391 subscribers
  • Views 325 views
  • Users 0 members are here
Related

Arduino - RFID/Keypad lock

Former Member
Former Member over 10 years ago

Hi,

 

I'd like to create a door lock using an electic strike place and have it activated by RFID or Pin.  The reason being that I don't want my kids to loose RFID tags and have to cancel them all the time so, they can use a pin.

 

I'm having trouble finding a combined RFID/KeyPad unit that is suitable.  I just want something that passes the info onto the Arduino so that I can manage it but the combined units I've seen so far use a Weigand format or protocol that I know nothing about.

 

Has anyone else done anything similar that can recommend a device?  I really don't want to have to separate the RFID and keypad.

 

These are the kind of things that I'm seeing - http://www.ebay.ie/itm/RFID-EM4102-Card-Reader-and-Keypad-Wiegand-26-for-EntryPro-/400717986567?pt=UK_Computing_Other_Computing_Networking&hash=item5d4ca73b07

 

Thanks,

 

Matt.

  • Sign in to reply
  • Cancel
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    There are Arduino libraries for reading Weigand signals available online.

     

    Another approach would be to issue your kids with a tag that would only work with a PIN, that means a lost token would be useless without the PIN, and the PIN could not be used to access the property on its own if divulged to others.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 10 years ago

    There are Arduino libraries for reading Weigand signals available online.

     

    Another approach would be to issue your kids with a tag that would only work with a PIN, that means a lost token would be useless without the PIN, and the PIN could not be used to access the property on its own if divulged to others.