Arduino
  • Products
  • More
Arduino
Arduino Forum Need help optimizing an LED design controlled by rotary switch
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 419 subscribers
  • Views 1347 views
  • Users 0 members are here
  • led
  • Charlieplexing
  • arduino
Related

Need help optimizing an LED design controlled by rotary switch

e14 Contributor
e14 Contributor over 11 years ago

Hello all I have a very specific project I am working on and while I have a working prototype I feel that there are things I can do to further optimize the design.

 

What it is


This is a simple feedback system for people to rate content they are watching live on a scale from -3-0-+3. The system consists of seven LEDs three red, followed by one blue and three green. These are controlled via a seven position rotary switch. I currently have this all plugged into gpio pins on an arduino mega and I would like to reduce the number of pins I am using. The reason I am using so many pins is I need to be able to light the leds sequentially i.e. three red, two red, one red, blue always on, one green, two green, three green. Meanwhile the Arduino program outputs the current selection over the serial port to a program that records this output.


What i want to do

 

Basically I want to reduce my pincount using Charlieplexing or some sort of led driver. I am currently using up 14 pins on the Arduino and I want to incorporate some other functions into this system. I am thinking charlieplexing is the answer but if there is a better solution I am open to suggestions!

 

Thanks in advance!

  • Sign in to reply
  • Cancel
  • D_Hersey
    0 D_Hersey over 11 years ago

    Another possibility would be to have a wafer switch switch out various resistors in the timing lag of an oscillator, then use a uP that is good at counting or phase detection to figure out where the switch is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 11 years ago in reply to e14 Contributor

    You could use the rotary switch with 7 resistors feeding a single analog input to indicate to the arduino which state is selected. Then you could de-multiplex 3 outputs from the arduino to implement the desired LED state.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    One great product is the attiny 85 with a the rotary charlieplex you can do everything you need as long as its less than 6 pins. The attiny uses arduino software and can be programmed with a few jumpers and an arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago

    As you can see, many ways to attack any one problem. Plan first and you will succeed. Like your avatar @Nick Santos

     

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<