Arduino Forum function in C++
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
  • State Verified Answer
  • Replies 12 replies
  • Answers 2 answers
  • Subscribers 395 subscribers
  • Views 733 views
  • Users 0 members are here
  • arduino
Related

function in C++

billpenner
billpenner over 10 years ago

When a function is finished, closed bracket}, where does the programming go?

My programming seems to fall through, that is the next function after the current function is complete seems to be running. Are incorrect brackets  causing my problem?

For example:

void loop() ;

{

do my first thing;

if test 1 true, go to void thing2

if test 2 true, go to void thing3

}

Where am I at this point? Am I back in the loop or do I fall through thing3 to what is after it in the program.

Please straighten me out a little. I am new to C++.

Thanks

Bill

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to gadget.iom +1 suggested
    OK, Call out the censors, he used the GOTO word…….. Ok, more seriously, GOTO is a bad thing to use and can leave you with a mess from a memory and cpu resource perspective, most modern languages do not…
  • mcb1
    mcb1 over 10 years ago in reply to Robert Peter Oakes +1
    GOTO is a bad thing to use and can leave you with a mess I know its disliked by some programmers, but I've seen others say there is nothing wrong with its use.... I guess there will always be opposing…
Parents
  • Former Member
    0 Former Member over 10 years ago

    With the semi-colon after the first line your loop will do nothing and therefore making the rest of the code void

     

    This should read

    void loop()

    {

    do my first thing;

    if test 1 true, go to void thing2;

    if test 2 true, go to void thing3;

    }

     

    The loop has no conditions so it will run forever

    1 - does "first thing"

    2 - test 1 (true) run thing2, then come back

    3 - test 2 (true) run thing3, then come back

    4 - start at top again

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    With the semi-colon after the first line your loop will do nothing and therefore making the rest of the code void

     

    This should read

    void loop()

    {

    do my first thing;

    if test 1 true, go to void thing2;

    if test 2 true, go to void thing3;

    }

     

    The loop has no conditions so it will run forever

    1 - does "first thing"

    2 - test 1 (true) run thing2, then come back

    3 - test 2 (true) run thing3, then come back

    4 - start at top again