Arduino Forum Powering JY-MCU HC06 Bluetooth adapter from the digital pin of an Arduino ??
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
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 401 subscribers
  • Views 856 views
  • Users 0 members are here
  • bluetooth
  • hc06
  • arduino
Related

Powering JY-MCU HC06 Bluetooth adapter from the digital pin of an Arduino ??

neilk
neilk over 10 years ago

I'm doing a lot of experiments with Arduino, Android and a JY-MCU HC06 Bluetooth adapter.


I'm becoming increasingly frustrated by the frequent need to reset the HC06, before it will accept a connection from the Android device. The easiest way to reset the HC06 is to briefly disconnect the +5V supply.

 

According to a spec of the HC06, which I found via Google, the HC06 draws 20-30mA when pairing up and 8mA in normal use. Since an Arduino Uno digital pin can supply 40 mA, wondered if I could power the HC06 from a digital pin, allowing me to reset the HC06 via software control of the digital pin.

 

Please can anyone offer any help or advice in this area?

 

Many thanks


Neil

  • Sign in to reply
  • Cancel

Top Replies

  • neilk
    neilk over 10 years ago in reply to clem57 +1
    Hi Clem Here is a photo of the Bluetooth adapter: At the moment, VCC isconnected +5 on the Arduino, and GND is connected to GND on the Arduino. I realise I could just put a switch in the +5 connection…
  • gadget.iom
    gadget.iom over 10 years ago in reply to neilk +1 suggested
    Substitute the relay coil connections with the Bluetooth module.
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    You could put a transistor between the arduino and the Bluetooth module just to be sure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • neilk
    0 neilk over 10 years ago in reply to gadget.iom

    Hi Paul

     

    Understand how to use a transistor to, say, drive a relay from an Arduino pin; don't quite understand how to use on for this application?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to neilk

    Substitute the relay coil connections with the Bluetooth module.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to neilk

    Substitute the relay coil connections with the Bluetooth module.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • neilk
    0 neilk over 10 years ago in reply to gadget.iom

    gadget.iom

     

    Thanks Paul, imagined it would be a bit more complicated than that image