Arduino Forum Two Arduinos in serial connection
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 392 subscribers
  • Views 360 views
  • Users 0 members are here
  • serial_connection
  • data_transfer
  • arduino
Related

Two Arduinos in serial connection

Former Member
Former Member over 10 years ago

Hi There

 

I want to send over a large integer over from one Arduino to the other through a serial connection. I know how to do this with a char, but a number like 234 and still having it as an integer on the Arduino send to, confuses me a bit. If someone could assist me with the code to do it, I'll appreciate it!

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • neilk
    0 neilk over 10 years ago

    Hi Andre

     

    If you have read the numeric characters - 234 in your question - , into a character array - call it numChar, then you can use the C++ standard library function atoi() to convert to an Integer - numInt = atoi(numChar);

     

    If the numeric characters have been read into a String Object, you can copy them to a character array using the standard Arduino function string.to CharArray() and then use atoi().


    I struggled with this problem myself. Hope it helps

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • neilk
    0 neilk over 10 years ago

    Hi Andre

     

    If you have read the numeric characters - 234 in your question - , into a character array - call it numChar, then you can use the C++ standard library function atoi() to convert to an Integer - numInt = atoi(numChar);

     

    If the numeric characters have been read into a String Object, you can copy them to a character array using the standard Arduino function string.to CharArray() and then use atoi().


    I struggled with this problem myself. Hope it helps

     

    Neil