Arduino Forum Setting Arduino Uno fuses
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
  • State Not Answered
  • Replies 10 replies
  • Subscribers 392 subscribers
  • Views 1057 views
  • Users 0 members are here
  • arduino
Related

Setting Arduino Uno fuses

gtrplyer16
gtrplyer16 over 10 years ago

All,

 

I have been working on a project lately which is an ATMega328p controlled power supply. I programmed the chip using the Arduino Uno board and I want to use a 16MHz crystal instead of the onboard 8MHz oscillator. I've been doing some research and people are saying I need to set fuses, but I'm not sure how to go about doing that. I only ran into this problem because I set up a 16MHz oscillator with 22pF caps and a 10k resistor and I was getting no clock signal into the chip. I downloaded the schematic from Arduino.cc and it showed to hook up my crystal across XTAL1 and XTAL2 and that's what I did and looking at those two pins on a scope I am getting 5V on the pins but it stays high. If someone could let me know if that would be a wiring problem or something different like setting fuses for example. This is my first project while using the ATMega328p out of the Arduino board so I'm having some troubles.

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago in reply to gtrplyer16 +1
    Take a look at the breadboard examples here: http://arduino.cc/en/Tutorial/ArduinoISP
  • sparky2k7
    sparky2k7 over 10 years ago +1
    Is this what you are trying to do? See link below. http://heliosoph.mit-links.info/arduinoisp-reading-writing-fuses-atmega328p/
Parents
  • sparky2k7
    0 sparky2k7 over 10 years ago

    Is this what you are trying to do? See link below.

    http://heliosoph.mit-links.info/arduinoisp-reading-writing-fuses-atmega328p/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gtrplyer16
    0 gtrplyer16 over 10 years ago in reply to sparky2k7

    I programmed the Mega328 while it was onboard the Uno. I then want to take that chip I programmed out and put into my circuit and have it work. My XTAL1 and XTAL2 pins go high to 5v and turn my display on however it stays high. I forgot to take a picture of my schematic today I was working on my radio design and it totally slipped my mind.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gtrplyer16
    0 gtrplyer16 over 10 years ago in reply to sparky2k7

    I programmed the Mega328 while it was onboard the Uno. I then want to take that chip I programmed out and put into my circuit and have it work. My XTAL1 and XTAL2 pins go high to 5v and turn my display on however it stays high. I forgot to take a picture of my schematic today I was working on my radio design and it totally slipped my mind.