Arduino Forum HELP PLEASE with sketch
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
  • State Not Answered
  • Replies 10 replies
  • Subscribers 404 subscribers
  • Views 725 views
  • Users 0 members are here
  • help
  • sketch
Related

HELP PLEASE with sketch

Former Member
Former Member over 10 years ago

I have a short 15 line sketch for a UNO.  It is to read a ultra sonic sensor and out put the results to the computer.  I will not compile. and has an error that I cannot find.  Is there some one who would be willing to help me find the problem.

 

If I knew how I would put it on the forum here if that would be OK.  I am not sure how to do that though.

  • Sign in to reply
  • Cancel

Top Replies

  • dtsartsanis
    dtsartsanis over 10 years ago in reply to Former Member +2
    Your code miss the void setup section put Serial.begin (9600); pinMode(trigPin, OUTPUT); pinMode(echoPin, INPUT); to void setup section and i believe will work
  • dmaruska
    dmaruska over 10 years ago in reply to clem57 +1
    I just did a search and found the HC-SR04 which used the Trig and Echo pins. I presume this is the sensor that he is using.
Parents
  • Former Member
    0 Former Member over 10 years ago

    #define trigPin 3

    #define echoPin 2

     

    void loop(){

      Serial.begin (9600);

      pinMode(trigPin, OUTPUT);

      pinMode(echoPin, INPUT);

     

      int duration, distance;

      digitalWrite(trigPin, HIGH);

      delayMicroseconds(1000);

      digitalWrite(trigPin, LOW);

      duration = pulseIn(echoPin, HIGH);

      distance = (duration/2) / 29.1;

      Serial.print(distance);

      Serial.print(" cm");

      delay(500);

    }

     

     

    it says there is an  undefined reference to 'setup'

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    You need the following:

     

    void setup(){

      }

    above void loop.

    This is code that runs one time! I would expect some commands like

      Serial.begin (9600);

      pinMode(trigPin, OUTPUT);

      pinMode(echoPin, INPUT);

    inside!

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dmaruska
    0 dmaruska over 10 years ago in reply to clem57

    Hi,  I have been looking at the code, and wondering what sensor are you using.  I have the Parallax sensor and could not get your code to work.  I made some changes and it works with this new code.  I have noticed that you have a trigger pin and a echo pin, this is the reason of my question. But with the Parallax this code works, the Parallax unit only has 3 pins, +5, GND and SIG. I also made a change on the Serial.print(" cm"); to include the "ln" to give it a line feed or return and start a new line.

     

    int trigPin = 3;

    //int echoPin = 2;

     

    void setup()

    {

      Serial.begin (9600);

    }

     

    void loop()

    {

      pinMode(trigPin, OUTPUT);

      //pinMode(echoPin, INPUT);

      long duration = 0;

      long distance = 0;

      digitalWrite(trigPin, LOW);

      delayMicroseconds(2);

      digitalWrite(trigPin, HIGH);

      delayMicroseconds(5);

      digitalWrite(trigPin, LOW);

      pinMode(trigPin, INPUT);

      duration = pulseIn(trigPin, HIGH);

      distance = (duration/2) / 29.1;

      Serial.print(distance);

      Serial.println(" cm");

      delay(500);

    }

     

    Regards,

     

    Dave M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to dmaruska

    This topic was for Arduino IDE using UNO from bobscnc. He said:

    It is to read a ultra sonic sensor and output the results to the computer

    The code may or may not work on any other environment. So your mileage may vary dmaruska

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to dmaruska

    This topic was for Arduino IDE using UNO from bobscnc. He said:

    It is to read a ultra sonic sensor and output the results to the computer

    The code may or may not work on any other environment. So your mileage may vary dmaruska

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dmaruska
    0 dmaruska over 10 years ago in reply to clem57

    I just did a search and found the HC-SR04 which used the Trig and Echo pins. I presume this is the sensor that he is using.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to dmaruska

    These are very common, so I think so. Here is a good view of one of these:

    Ultra01_01

    http://www.elecfreaks.com/244.html


    Clem