Arduino Forum Need to hack adafruit motor shield V1
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
  • State Not Answered
  • Replies 0 replies
  • Subscribers 390 subscribers
  • Views 190 views
  • Users 0 members are here
  • hack
  • arduino
Related

Need to hack adafruit motor shield V1

Anonymous-241635
Anonymous-241635 over 10 years ago

i have a adafruit motor shield v1 and i need to hack the code to enable me to attached a second one to it using the arduino analogue pins.

one shield allows me to control up to 4 DC motors and i need to control 6 DC motors

any suggestions would be great

i have looked at the pins being used and the ones not being used so i know the theory behind it but when i look at the code to run the shield i do not know what to edit to allow me to use the analogue pins