Arduino Forum Help with Digital Pins and TFT Display
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
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 402 subscribers
  • Views 923 views
  • Users 0 members are here
  • digital_pins
  • programming
  • tft-lcd
  • digital-to-analog
  • arduino
  • newbie
Related

Help with Digital Pins and TFT Display

Former Member
Former Member over 10 years ago

Is it "syntaxly" correct if I plug in "digitalRead" wherever I see "analogRead" in a code meant to read from an analog pin? I'm trying to make my TFT LCD read from a digital pin, but I could find was a code that helped it read from an analog pin (http://arduino.cc/en/Tutorial/TFTDisplayText).

 

I'm using the analog version of that code to print information from a temperature sensor to the TFT LCD, but I'd also like to print values from ultrasonic range finder (URF) -- that uses a digital pin. At first, the URF and TFT LCD needed the same digital pin (pin 7) according to the code I used. I figured I couldn't get the digital value to print because the two used the same pin--since the URF didn't work when using any other pin, I switched the "cs" pin of the TFT to digital pin 4. It still displays fine, other than the absence of the URF's value.

 

Context:

- Board: Arduino Leonardo

- TFT Display/LCD Module with SD Card Reader (http://arduino.cc/en/Main/GTFT)

- Serial Port: /dev/tty.usbmodem1421

- Arduino version 1.0.6

- Goal: get TFT LCD to read from ultrasonic range finder.

 

Thanks for any replies in advance!

 

My Code: (I deleted the serial print parts and all others I deemed not relevant)

//create an instance of the library

TFT myScreen = TFT(cs, dc, rst);

 

// char array to print to the screen

char tempPrintout[6]; //[4] gives xx._, [5] gives xx.x

 

char soundPrintout[6]; //****For the URF!

 

void setup() {

....

Serial.begin(9600);

 

}

 

void loop() {

 

  // Read the value of the sensor on A1 (Temp sensor)

  String tempVal = String(analogRead(A1)* 0.48828125);

 

  // convert the reading to a char array

  tempVal.toCharArray(tempPrintout, 6); //changes decimal places

 

    // Read the value of the sensor on.....pin 7???

  String soundVal = String(digitalRead(pingPin)); //this doesn't work

 

  //convert the reading to a char array

  soundVal.toCharArray(soundPrintout, 6); //not sure if this should work

 

... //coding to format text

 

  // establish variables for duration of the ping,

  // and the distance result in inches and centimeters:

  long duration, cm; //inches

 

  // The PING))) is triggered by a HIGH pulse of 2 or more microseconds.

  // Give a short LOW pulse beforehand to ensure a clean HIGH pulse:

  pinMode(pingPin, OUTPUT);

  digitalWrite(pingPin, LOW);

  delayMicroseconds(2);

  digitalWrite(pingPin, HIGH);

  delayMicroseconds(5);

  digitalWrite(pingPin, LOW);

 

  // The same pin is used to read the signal from the PING))): a HIGH pulse whose duration is the time (in microseconds) from the sending of the ping to the reception of its echo off of an object.

  pinMode(pingPin, INPUT);

  duration = pulseIn(pingPin, HIGH );

 

  myScreen.text(soundPrintout, 10, 40); //???

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +1 suggested
    A digitalRead on a pin determines is it on or off. Just two values. Do you have only two values for Temp? Looking at analogRead , the values returned are a range from say 0 to 1023. They convert analog…
  • clem57
    0 clem57 over 10 years ago

    A digitalRead on a pin determines is it on or off. Just two values. Do you have only two values for Temp? Looking at analogRead , the values returned are a range from say 0 to 1023. They convert analog to digital (ADC) and approximate as close as possible. On the arduino only pins labeled as PWM are analog capable. Look at datasheet for ultrasonic range finder (URF) to determine should it be digital or analog and pick the correct type. The variable pingPin should be set to that pin you physical set.

    Cheers,

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Temp has a range of values, I actually use it to tell the temperature, after multiplying the value by 0.41.... The URF datasheet says that it should be connected to pin 7, so I declared that in the beginning. I tried plugging it into an analog pin, but it didn't work. Apparently, pin 7 on the arduino leonardo is labeled as PWM. In that case, I'll try converting the digital pin to an analog one: but should I be trying to change the nature of the pin or the data the pin returns (if that makes sense)?

     

    Thanks!