Arduino Forum GPS
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
  • State Not Answered
  • Replies 7 replies
  • Subscribers 405 subscribers
  • Views 590 views
  • Users 0 members are here
  • &
  • servo
  • gps
  • arduino
  • r/c
Related

GPS

Former Member
Former Member over 10 years ago

I was thinking about making a radio control boat about 30 inches (76 CM) long.  I would want to use the R/C unit to set a course then let the GPS to keep it on course.  I would want it to also be able to return to the launch point when I give it a signal.

It seems that this should be possible using an arduino, R/C servo and a GPS unit

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago +1
    Have you seen this site Random Tech Stuff: Experiments with the RFM69 433MHz digital transceiver module it uses a custom chip but does have some of what are looking for.
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    An arduino could do it but with limited ram etc, it may be reduced to a very basic set of way points and not tracking intermediate spots. going home would be a case of either reversing the ay point order…
Parents
  • clem57
    0 clem57 over 9 years ago

    Did this go anywhere?BOB NELSON

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago

    Did this go anywhere?BOB NELSON